Skip to main content
Associate
Nov 26, 2025 11:58 AM UTC
Solved

Missing 'External loaders' in Debugger tab

Hello,

I've recently created an External Loader to be used on a TouchGFX project (H563 with SPI LCD and SPI external flash). When I use this loader in Cube Programmer, it programs the processor and SPI flash, and runs as expected. So now I want to add it into my project in CubeIDE. Normally I would find the External Loaders under the Debugger tab (between SWV and Misc) but this seems to be missing. Is there a way to enable this?

st ext ld.jpg

(This project was created un der CubeIDE 2.0.0, but this section also is missing in projects created by previous versions. Example projects created from TouchGFX does have this section).

Any ideas?

PP22

ST Technical Moderator
Nov 26, 2025 12:44 PM UTC

Hello @PP22 

 

Let me thank you for posting.

To add the external loader, you need to select ST-Link (ST-LINK GDB server) or ST-LINK (OpenOCD) as Debug probe.

MahmoudBenRomdhane_0-1764160979732.png

MahmoudBenRomdhane_1-1764161033471.png

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
Nov 26, 2025 12:44 PM UTC

Hello @PP22 

 

Let me thank you for posting.

To add the external loader, you need to select ST-Link (ST-LINK GDB server) or ST-LINK (OpenOCD) as Debug probe.

MahmoudBenRomdhane_0-1764160979732.png

MahmoudBenRomdhane_1-1764161033471.png

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PP22Author
Associate
Nov 26, 2025 1:23 PM UTC

Hi Mahmoud,

Thanks for the prompt reply.

 

Now you mention it, my projects showing 'External Loader' were on Nucleo boards using ST-Link so that clears up that bit of confusion.

Is this not available with a Segger J-Link? (when I used CubeProgrammer I select JLink/Flasher as the probe).

Is it possible use the J-Link to program the H563 and external SPI flash via CubeProgrammer CLI?

PP22

 

 

 

PP22Author
Associate
Dec 2, 2025 6:02 AM UTC

Sorted now using CubeProgrammer CLI.