Skip to main content
PEnde.1
Associate
August 28, 2021
Solved

Migrated from STM32CubeIDE V1.6 to CubeIDE V1.7 and now an F103C6T6 application refuses to debug consistently and continuously resets. Using RTOS, CAN and timers 1 & 3. Any ideas

  • August 28, 2021
  • 3 replies
  • 1230 views

..

This topic has been closed for replies.
Best answer by PEnde.1

Found it. It seems that by default the IWDG is on so is causing resets. Solved by including the IWDG initialisation and servicing resets to it in the main thread. Something must have changed in the startup(F103C6tx) to have done this as this project was working properly when built with MXCubeIDE V1.6.0

Anyway all solved and working again. I guess having the watchdog running isn't such a bad thing anyway.

3 replies

TDK
August 28, 2021

> F103C6T6

knock-off chip and/or programmer?

> refuses to debug consistently

Perhaps provide a more detailed description.

> continuously resets

Determine the cause of the reset in RCC->CSR.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PEnde.1
PEnde.1Author
Associate
August 28, 2021

Could only be a knock off chip and / or programmer if Farnell are supplying knock offs which I very much doubt. This worked perfectly prior to updating from V1.6.1 to 1.7.0. RCC_CSR shows reset being caused by Low Power management and software resets. (I had already been down that path).

PEnde.1
PEnde.1AuthorBest answer
Associate
August 29, 2021

Found it. It seems that by default the IWDG is on so is causing resets. Solved by including the IWDG initialisation and servicing resets to it in the main thread. Something must have changed in the startup(F103C6tx) to have done this as this project was working properly when built with MXCubeIDE V1.6.0

Anyway all solved and working again. I guess having the watchdog running isn't such a bad thing anyway.