Skip to main content
AWarr.1
Associate
August 17, 2022
Question

MCU Finder still doesn't work, despite the release notes saying that it was fixed.

  • August 17, 2022
  • 3 replies
  • 1641 views

The 1.8 release notes claim that the wayland support bug was fixed, yet the mcu finder still doesn't work. Please reopen bug 77518 or fix the issue.

This topic has been closed for replies.

3 replies

Aymen CHAKROUN
ST Employee
August 17, 2022

Hi @AWarr.1​ ,

Can you please open the CubeIDE installation folder and right click the file 'stm32cubeide_wayland' and select 'Run as a Program'.

Regards,

Aymen.

AWarr.1
AWarr.1Author
Associate
August 30, 2022

As far as I can tell, this executable is only delivered with the generic linux build. I am using the rpm installer.

Semer CHERNI
ST Employee
August 30, 2022

Hello @AWarr.1​ 

Did the proposition of @Aymen CHAKROUN​  came to help?

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.