Skip to main content
Associate II
Jan 15, 2025 3:34 PM UTC
Solved

Managing multiple configurations

Originally a reply to this, but is a separate discussion.


I've been playing with build configurations, working set, etc, for a while.

I know it's Eclipse and CDT's fault, not STM's. But it's SOOOOOOOO confusing, and there must be a solution. So far, I've created "things", mostly empty, useless "things" : Build Targets, Working Sets, etc. None cause a build to behave as expected.

Which is : having multiple "thing" "target" "thingies", each one using its own linker script (and why not, later at some point, specific .h/.c files). And being able to build one, or another, to get different FWs, each one using its own FLASH ORIGIN settings. Better even would be : one build, multiple FWs, each one in its own folder using its own linker script.

What's behind : OTA. As far as I understood, the linker script is the only place where a FW get its boot address. So far, when I build a FW #2, flash it in the second flash bank, the MCU boots the FW #1 from the first flash bank as long as the linker script indicates

 

FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K

 

I have to build FW #1 with this ORIGIN, then change ORIGIN by hand, then build FW #2. And not forget to copy FW #1 before build FW #2.

There must be a way to automate such builds ?

This topic has been closed for replies.
Associate II
Jan 15, 2025 4:01 PM UTC

Oh yes, thanks, that does the job.

Well, can I add another level ? Is it possible to launch several builds with one click ?

4 replies

Andrew Neil
Super User
Jan 15, 2025 3:49 PM UTC

To answer your question, "Would it be possible to set one specific linker script per Build Configuration?" here:

Yes.

The Linker script is specified here - it is subject to the Configuration setting:

AndrewNeil_0-1736956125208.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Christophe BeugnetAuthorBest answer
Associate II
Jan 15, 2025 4:01 PM UTC

Oh yes, thanks, that does the job.

Well, can I add another level ? Is it possible to launch several builds with one click ?

Andrew Neil
Super User
Jan 15, 2025 4:19 PM UTC

Not tried it myself, but:

AndrewNeil_0-1736957873288.png

I think this is all standard Eclipse stuff - so googling for general Eclipse documentation etc would probably be worthwhile...

 

PS:

The 'Build Selected...' goes to:

AndrewNeil_1-1736958010788.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Jan 16, 2025 12:52 AM UTC

OK, tested and working, thanks
I missed this one too

I also did search "The Internet" for eclipse + CDT + build configurations or targets, etc. But DuckDuckGo is not my friend ...