Skip to main content
chriskuku
Senior II
May 22, 2026 5:19 PM UTC
Question

Main Config: ... have some not configured or wrong parameter values[FREERTOS]

I was running a project in STM32CubeIDE (1.19.0) with 4 Tasks and it ran fine. Now I wanted to add a fifth task and after adding it and the oly thing I had changed was the Name (Task05 instead of myTask05) I got an alert box when saving the .ioc file:

Bildschirmfoto 2026-05-22 um 10.12.51.png

I went with this into the FreeRTOS forum, but they say it's an STMicro issue. So I'm coming up with it here now.

1 reply

Pavel A.
May 22, 2026 10:50 PM UTC

Changes in generated code should be done with caution (in the "USER CODE" sections, etc.)

Better move as much as possible of the custom code out to your own files. For example, let the generated code create only the main task, and create all other tasks and other objects in your own file.