Skip to main content
rclar.6
Associate III
Apr 21, 2026 7:13 AM UTC
Solved

login need for code generation hidden

So apparently in 2026, creating a basic embedded C project now requires… a login.

Tried spinning up a project in STM32CubeIDE and got a nice “half-built” result:

  • Project created ✔
  • Code generation :cross_mark:
  • Explanation :cross_mark:

Turns out the IDE now needs to quietly download the HAL/CMSIS packages, which in turn requires a myST account login… but:

  • It doesn’t tell you that
  • It doesn’t prompt you (on Linux at least)
  • It just silently fails and leaves you debugging yourself

So you end up thinking:
“Did I misconfigure the clock? The linker script? The .ioc?”

Nope. You just weren’t logged into a website.

Nothing says robust embedded tooling like a hidden cloud dependency for generating main.c.

Bonus points for the UX where the “login” option is buried under:
Help → STM32Cube Updates → Connection to myST

Because obviously that’s the first place you look when your GPIO project won’t build.

Anyway—manual firmware download and local install fixes it. Once you discover the secret handshake.

Progress :thumbs_up:

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Apr 21, 2026 7:39 AM UTC

Hello @rclar.6 

Please try to use the latest version of STM32CubeMX6.17.0 and STM32CubeIDE 2.1.1 ,in which  the ST login feature has been removed from the user interface.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Apr 21, 2026 7:39 AM UTC

Hello @rclar.6 

Please try to use the latest version of STM32CubeMX6.17.0 and STM32CubeIDE 2.1.1 ,in which  the ST login feature has been removed from the user interface.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.