Skip to main content
Associate
May 15, 2024 9:20 PM UTC
Solved

Login issue - STM32CubeIDE and STM32MX

I downloaded version 1.15.1 of the STM32 IDE, but when I start a new project and select the STM32F103C8T6 as the MCU, the first image appears. However, when I try to update the firmware, it asks for a login, and the second image appears. I have searched in several places and realized that this is an error that can occur since versions 1.12/1.13. I have tried changing the network connections to active provider (native, manual, and direct), but it doesn't work. (I'm not sure how the manual one works, but I also saw that it's not good to keep using manual mode). Does anyone have any suggestions? The same problem occurs in STM32MX, and I have also tried changing the internet connection.

inouee_0-1715807624184.png (First image)

inouee_1-1715807726813.png(second image)

 

    This topic has been closed for replies.
    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    May 16, 2024 5:48 PM UTC

    Dear all,

    This is an issue some CubeMx/CubeIDE users are facing since yesterday and the issue was escalated internally to be fixed asap. Dedicated teams are working on it.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

    19 replies

    Visitor II
    Dec 27, 2024 10:23 AM UTC

    This problem still remains for 1.17.0 cubeIDE for Mac and Windows.