Skip to main content
CSmit.4
Associate II
October 11, 2024
Solved

Loading code on STM32U535 vs STM32U545

Hello, we have an STM32CubeIDE project based on the STM32U545. Unfortunately, our first version of PCB's is due to arrive soon populated with the STM32U535 instead, due to parts shortages. My question is, can I use the IDE to load and debug the code as is, or do I need to create a different project based on the STM32U535. The two parts are almost identical, except for the crypto engine, which we arent using yet, so I am not concerned about binary compatability, just whether the IDE will complain when it sees a 535 instead of a 545.

    This topic has been closed for replies.
    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    October 11, 2024

    Hello @CSmit.4 ,

    Yes you can upload your application as it is on STM32U535 instead of STM32U545 if you are not using Crypto feature.

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

    1 reply

    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    October 11, 2024

    Hello @CSmit.4 ,

    Yes you can upload your application as it is on STM32U535 instead of STM32U545 if you are not using Crypto feature.

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.