Skip to main content
thln47
Associate III
October 25, 2022
Solved

Linker error using static library

Hello,

I use an open source projet (open62541 on github) to get OPC-UA implementation over lwip.

When my projet is compiled with open62541 source code, it's works without error.

But the 2 files generated 'open62541.c' and 'open62541.h' are very big (around 4 and 1 Mbytes).

My cross compiler is gcc form STM32CubeIDE Version 1.9

   GNU Tools for STM32 (10.3-2021.10)

   arm-none-eabi-gcc -v    

Using built-in specs.
OLLECT_GCC=arm-none-eabi-gcc
COLLECT_LTO_WRAPPER=c:/st/stm32cubeide_1.9.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/lto-wrapper.exe
Target: arm-none-eabi
Configured with: /build/gnu-tools-for-stm32_10.3-2021.10.20211105-1100.....
Thread model: single
Supported LTO compression algorithms: zlib
gcc version 10.3.1 20210824 (release) (GNU Tools for STM32 10.3-2021.10.20211105-1100)

To optimize my compilation operation, I want to make a library for open62541 functions.

I compile open62541 source code to get a libopen62541.a file, then I link this library with my projet.

I've some linker error, as you can see below:

arm-none-eabi-gcc -o "STM32_TBUS.elf" @"objects.list" -lmbedtls -lopen62541-mbedtls -mcpu=cortex-m7 -T"D:\ST\STM32CubeIDE\workspace\STM32_TBUS\STM32H743ZITx_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32_TBUS.map" -Wl,--gc-sections -static -L"D:\ST\STM32CubeIDE\workspace\STM32_TBUS\Lib\mbedtls" -L"D:\ST\STM32CubeIDE\workspace\STM32_TBUS\Lib\OPC-UA" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
 
 c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: D:\ST\STM32CubeIDE\workspace\STM32_TBUS\Lib\OPC-UA\libopen62541-mbedtls.a(open62541.o): in function `ServerNetworkLayerTCP_close':
 
 open62541.c:(.text.ServerNetworkLayerTCP_close+0xc): undefined reference to `lwip_shutdown'
 
 c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: D:\ST\STM32CubeIDE\workspace\STM32_TBUS\Lib\OPC-UA\libopen62541-mbedtls.a(open62541.o): in function `connection_write':
 
 open62541.c:(.text.connection_write+0x30): undefined reference to `lwip_send'
 
 c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: open62541.c:(.text.connection_write+0x52): undefined reference to `lwip_poll'
 
 c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: D:\ST\STM32CubeIDE\workspace\STM32_TBUS\Lib\OPC-UA\libopen62541-mbedtls.a(open62541.o): in function `connection_recv':
 
 open62541.c:(.text.connection_recv+0x50): undefined reference to `lwip_select'
 
 ...
 
 

I suspect that functions called from library are not correctly linked, perhaps the optimizer remove some function not use from the main code.

But theses functions are used from the library.

--[ main_code ] --> [open62541 library] ---|
--[ lwip stack ] < ------------------------|

The functions not found are those of lwip.

If anyone has any idea, thanks for your help.

This topic has been closed for replies.
thln47
thln47Best answer
Associate III
October 26, 2022

Thanks "Pavel A.", but I found my problem.

When I made the libopen62541.a library, I've forget to define LWIP_COMPAT_SOCKETS with value 2.

So lwip functions was undefined, and when I link the library with my main project, the linker failed.

2 replies

thln47
thln47AuthorBest answer
Associate III
October 26, 2022

Thanks "Pavel A.", but I found my problem.

When I made the libopen62541.a library, I've forget to define LWIP_COMPAT_SOCKETS with value 2.

So lwip functions was undefined, and when I link the library with my main project, the linker failed.