Skip to main content
pclem
Associate
May 4, 2019
Question

'Launching STM32L476RG_nucleo.elf has encountered a problem. Error starting process'

I am on a windows 7 PC and used to work with MBED, then AC6 SW4STM32 without problem with an own made card with a L476RG mcu.

I downloaded STM32IDE to test it, the installation ok without problem.

I uploaded a very simple program called GPIO_IOT_toggled from examples. The building works fine. At the time to run the program, I choose "run as "local C/C++ application" (the only choice).

A little window says:

'Launching STM32L476RG_nucleo.elf has encountered a problem. Error starting process'

When clicking on "details" I get:

"Cannot run program "C:\Users\YPCU5336\STM32Cube\Repository\STM32Cube_FW_L4_V1.14.0\Projects\NUCLEO-L476RG\Examples\GPIO\GPIO_IOToggle\SW4STM32\STM32L476RG_NUCLEO\Debug\STM32L476RG_NUCLEO.elf": Launching failed"

Can someone tell me if I missed some tuning in the STM32CubeIDE ?

Thank you in advance

This topic has been closed for replies.

2 replies

Markus GIRDLAND
ST Employee
May 6, 2019

When you mention you upload the CPIO_IOT_toggled program did you import it from SW4STM32 format to CubeIDE in that process?

I've tried a similar example (on a NUCLEO-L4R5ZI) and it seems to be working for me.

Could you activate the gdb server log in your debug configuration and paste that for me?

pclem
pclemAuthor
Associate
May 20, 2019
Hi Markus, Sorry for the delay, I had to travel overseas... I activated the GDB server log, you can find this trace enclosed. When I launch "RUN as", I see one only option : "local C/C++ Application" that leads to a choice of 2 options: a- STM32L476RG_nucleo debug b- STM32L476RG_nucleo.elf each of these options don't work and the choice 2 leads to the previously described error message When I launch "debug as", I see 2 options: 1- "local C/C++ Application" 2- "STM32 MCU C/C++ application" each of these 2 options lead to options a et b above When choosing option b, the same error message when choosing option a, it works (I enter debug mode, when I quit debug the program works normally) One more point: I tried to avoid going through "RUN as" or "DEBUG as" by dragging and dropping the executable .bin directly to my STLINK Node_L476RG representation in the file explorer, and THAT WORKS. Thank you for your time Philippe <> Garanti sans virus. www.avast.com <> <#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>