Skip to main content
Associate III
April 22, 2024
Solved

Join a font in a main.C

Hi everybody,

 

After several attempts, I cannot correctly declare my variables in the files. I'm a little lost with file declarations to reach certain variables delcared elsewhere

This is why I decided to come and ask for help.

 

I 'm actually work on a screen with st7567 driver.

For that I have create à font.h to stock some font : like this

 

 

 

 

// Character bitmaps for Microsoft Sans Serif 10pt
const uint8_t microsoftSansSerif_10pt[] =
{
	// @0 '!' (1 pixels wide)
	// #
	// #
	// #
	// #
	// #
	// #
	// #
	// #
	//
	// #
	0xFF,
	0x02,

	// @2 '"' (3 pixels wide)
	// # #
	// # #
	// # #
	// # #
	0x0F, 0x00, 0x0F,

 

 

 

 

 

after I have create a driver to communciate with the st7567 driver.

I have call this files st7567_driver.h and st7567_driver.c .

In the st7567_driver.c I declared file like this :

 

 

 

 

/**************************************************************************************
 * Included Files
 **************************************************************************************/

#include <stdint.h>
#include <stdbool.h>
#include <string.h>

#include "stm32l031xx.h"
#include "main.h"
#include "st7567_driver.h"
#include "font.h"


extern SPI_HandleTypeDef hspi1; // Je mets extern pour signifier que la déclaration de la fonction est ailleurs ( dans le main.c)

 

 

 

 

 

Now the problem begin because I'm A noob :

 

In my main.c , I would like to use a function which sends the name of the font to use.

 

 

 

 

 Draw_text(0,0,'K', &microsoftSansSerif_10pt);

 

 

 

 

 

microsoftSansSerif_10pt is the name of my font in the font.h

 

But the comoler send me an error :

../Core/Src/main.c:110:23: error: 'microsoftSansSerif_10pt' undeclared (first use in this function)

 

I tried several ways to do it with the words "extern" to declare antoher file etc...

I also read the documentation, but I did not succeed in understanding the process.

 

IF someone who knows this subject well could guide me on how and where to declare the files that would be super nice.

Thank you vcery much

dje8269

 

    This topic has been closed for replies.
    Andrew Neil
    Andrew NeilBest answer
    Super User
    April 22, 2024

    @JJoao.1 wrote:

    After several attempts, I cannot correctly declare my variables in the files. I'm a little lost with file declarations to reach certain variables delcared elsewhere

     


    This is standard C programming stuff:

    https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/657455/highlight/true#M25847

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

    7 replies

    AScha.3
    Super User
    April 22, 2024

    Hi,

    how did you get your files to the project ?

    -> You have to "import" them, so the IDE/compiler knows, they are part of project now:

    right click on folder to import -> file system-> select directory: files to import ; 2x , for .h and .c then.

    Then compile again...

    If you feel a post has answered your question, please click on " Best Answer ".
    JJoao.1Author
    Associate III
    April 22, 2024

    Thank you for the reply AScha.3 ,

    I created them and not imported them

    I wonder if I should create a font.c instead of font.h

    AScha.3
    Super User
    April 22, 2024

    oooo, just if you have .h and c. files !!! Only import, what you need. :)

     

    If you feel a post has answered your question, please click on " Best Answer ".
    mƎALLEm
    ST Technical Moderator
    April 22, 2024

    Create font.c file and put your fonts declaration there.

    in font .h export these fonts as extern.

    in main.c include font.h.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Andrew Neil
    Andrew NeilBest answer
    Super User
    April 22, 2024

    @JJoao.1 wrote:

    After several attempts, I cannot correctly declare my variables in the files. I'm a little lost with file declarations to reach certain variables delcared elsewhere

     


    This is standard C programming stuff:

    https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/657455/highlight/true#M25847

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    mƎALLEm
    ST Technical Moderator
    April 22, 2024
    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    JJoao.1Author
    Associate III
    April 22, 2024

    Thank you s omuch for your answwers !

    I think I succeeded!


    I redid the configuration as in the link sent by Andrew Neil.
    I had to create a .c and a .h file

    In the .h i declared extern variable

    in my .c file I write my font normaly.

    And in my Main.c I include font.h

     

    Thank you so much