Visitor II
Jun 10, 2026 8:55 AM UTC
Question
ITM Debug issue in STM32G474VET6
- 0 replies
- 42 views
I am working with an STM32G474 and trying to enable ITM/SWV trace using STM32CubeIDE and ST-LINK.
Configuration
- MCU: STM32G474
- STM32CubeMX
- Debug Mode: Trace Asynchronous SW (SYS → Debug)
- Default HAL initialization generated by CubeMX
i have atteched the .ioc file .
Issue
After changing the debug configuration from Serial Wire to Trace Asynchronous SW, the application gets stuck inside:
HAL_Delay(500);The program never returns from HAL_Delay().
Observations
SysTick_Handler() is present and contains:
void SysTick_Handler(void)
{
HAL_IncTick();
}However, when debugging, it appears that the HAL tick is not progressing, causing HAL_Delay() to wait indefinitely.
I found several discussions mentioning:
- Moving the HAL time base from SysTick to TIM6/TIM7
- Checking the TIM6 interrupt priority
- Ensuring the correct
HAL_InitTick()implementation is used
Questions
- Is there any known issue or required configuration when enabling Trace Asynchronous SW (ITM/SWV) on STM32G474?
- Can enabling SWV trace affect the HAL tick source or SysTick operation?
- Is it recommended to switch the HAL time base to TIM6 when using ITM/SWV?
- What is the recommended CubeMX configuration for using ITM trace while keeping
HAL_Delay()functional?
Any suggestions on how to diagnose why the HAL tick stops after enabling SWV trace would be greatly appreciated.
Thank you.