Skip to main content
Associate
November 15, 2023
Solved

issue with fmaf function

Hallo,

I used in my app fmaf function and I found it doesn't behave as expected:

y = fmaf(a1,a2,a3) should be y = a1*a2 + a3

but I got as result y = a1*a2 without additive term.

Of course I can and use "classic" expresion instead this functions.

Is this a bug or maybe I misunderstood something?

I'm using STM32CubeIDE 1.13.2, and STM32F401ceu...

Greg

 

Below is also dissasembled piece of code:

 

137 q = fmaf(0.98564736f, D, 280.459f);
080014ea: vldr s2, [pc, #200] ; 0x80015b4 <Sun_Longitude_Deg+332>
080014ee: vldr s1, [r7, #4]
080014f2: vldr s0, [pc, #188] ; 0x80015b0 <Sun_Longitude_Deg+328>
080014f6: bl 0x800c8d0 <fmaf>

fmaf:
0800c8d0: vfma.f32 s0, s0, s1
0800c8d4: bx lr
0800c8d6: movs r0, r0
__ieee754_atan2:

 

    This topic has been closed for replies.
    STTwo-32
    STTwo-32Best answer
    ST Technical Moderator
    November 17, 2023

    Hello again @KwA 

    I've just tested your code and i Can confirm the issue. As a workaround, you Can use fma (i've tested and it works fine).

    PS : i've done my test using CubeIDE 1.13.2.

    Best Regards.

    STTwo-32 

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    8 replies

    STTwo-32
    ST Technical Moderator
    November 15, 2023

    Hello @KwA and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    I can't reproduce that issue. Can you share your code here so we may can find the problem.

    Best Regards.

    STTwo-32 

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    KwAAuthor
    Associate
    November 15, 2023

    Hello, yes I can share but I think it is unusable in this form. I just use normal expression insted of fma. This all fma callings are commented out.

    Sorry, the code looks terrible - I don't know how to make this formated here:

     

    float Sun_Longitude_Deg(float D) {
    float g, q, L;
    float gr;

    // g, q, and L are in degrees
    // Mean anomaly of the Sun:
    g = 357.529f + 0.98560028f * D;
    //g = fmaf(0.98560028f , D, 357.529f);

    if (g >= 360) //while (g > 360)
    { //g -= 360;
    g = fmodf(g, 360);
    } else {
    while (g < 0) { g += 360;}
    }

    // Mean longitude of the Sun:
    q = 280.459f + 0.98564736f * D;
    //q = fmaf(0.98564736f, D, 280.459f);
    if (q >= 360) //while (q > 360)
    { //q -= 360;
    q = fmodf(q, 360);
    } else {
    while (q < 0) { q += 360;}
    }

    // Sun's geocentric apparent ecliptic longitude (adjusted for aberration):

    gr = D2R(g);
    L = q + 1.915f*sinf(gr) + 0.020f*sinf(2*gr);

    //L = fmaf(1.915f, sinf(gr), q);
    //L = fmaf(0.020f, sinf(2*gr), L);

    return L;
    }

    Tesla DeLorean
    Guru
    November 15, 2023

    Yes looks broken, although the Keil output has __hardfp_fmap which is much more complex

     0x08003eda: ed9f0a0c .... VLDR s0,[pc,#48] ; [0x8003f0c] = 0x3f7c5363
     0x08003ede: eddf0a0c .... VLDR s1,[pc,#48] ; [0x8003f10] = 0x42f6e666
     0x08003ee2: ed9f1a0c .... VLDR s2,[pc,#48] ; [0x8003f14] = 0x438c3ac1
     0x08003ee6: f000f829 ..). BL __hardfp_fmaf ; 0x8003f3c

     

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    November 15, 2023

    With GNU 4.93 something similar

    f = fmaf(0.98564736f, f, 280.459f);
    
     0x080015e4: ed9d7a02 ...z VLDR s14,[sp,#8]
     0x080015e8: eddf6a23 ..#j VLDR s13,[pc,#140] ; [0x8001678] = 0x3f7c5363
     0x080015ec: eddf7a23 ..#z VLDR s15,[pc,#140] ; [0x800167c] = 0x438c3ac1
     0x080015f0: 481b .H LDR r0,[pc,#108] ; [0x8001660] = 0x80084ef
     0x080015f2: eee67a87 ...z VFMA.F32 s15,s13,s14
     0x080015f6: edcd7a02 ...z VSTR s15,[sp,#8]
    
     printf("%f\n", f);
    
     0x080015fa: eddd7a02 ...z VLDR s15,[sp,#8]
     0x080015fe: eeb77ae7 ...z VCVT.F64.F32 d7,s15
     0x08001602: ec532b17 S..+ VMOV r2,r3,d7
     0x08001606: f002fb81 .... BL printf ; 0x8003d0c
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    KwAAuthor
    Associate
    November 15, 2023

    in this dissasembly it looks like VFMA is operating on three different registers contrary to my where it operates on two different registers (omits s2 in my case).