Skip to main content
KKane
Associate II
December 13, 2019
Question

Issue when clone the project in STM32CubeIDE

Dear Sirs,

I copy and pasted to clone the project in project explorer window of STM32CubeIDE.

And some cases "Src" folder is automatically deleted from original project folder.:grinning_face_with_sweat:

Does anyone faced similar issue ? and how can I clone the project safely in STM32CubeIDE ??

Best regards,

K. Kaneko

This topic has been closed for replies.

22 replies

Hvan .2
Associate
February 19, 2020

Hi Kazu,

I did not have that problem... To check for you I just redid all the steps I took and wrote them down for you. Maybe you find the solution here:

-right clicked on project in STM32CubeIDE Project explorer

-I chose copy and pasted the project on desktop

-renamed the project folder

-opened the project folder and edited the .project file with Notepad++

-changed the <name> old name <name> section to <name> new name <name>

-I went back to STM32CubeIDE, right clicked on an empty part of Project Explorer and chose Import

-in the import dialog box I chose 'Existing Projects into Workspace'. Then clicked Next.

-in the Root Directory section I browsed to the copied folder on my desktop. Then clicked Finish

-right clicked on empty part of Project Explorer and chose Refresh (just for certainty's

sake (doesn't appear necessary as the project name was visible straight away))

-right clicked on the copied project folder and clicked Clean. Console displayed: make -j4 clean, 

rm -rf * and then finished

-all of the files (Core: Inc, Src, Startup) were present and I could build the project correctly with no

errors or warnings

-I could debug the project correctly. After stopping the debug there was no cross-linkage of the

startup .s file like I had before. So seeing all this Pavel's method appears to work perfectly!

I hope this helps Kazu!

Heiko

KKane
KKaneAuthor
Associate II
February 19, 2020

​Hello Heiko,

Many thanks for your whole procedure.

I followed step by step, but in the end when I modify .ioc file in CubeMX view and save/generate code in copied new project, main.c file still deleted from original project folder...

I'm using STM32CubeIDE  1.2.0 and installed DevStyle dark view and may be some side effect by such add-ons.

I will try to newly install CubeIDE into another PC and check if situation changes.

Best Regards !

Kazu

Hvan .2
Associate
February 20, 2020

Hi Kazu!

I had time to look at what you reported. You are right!

I noticed in my copied project that the .ioc and .launch file still had the old name.

I renamed them just to be sure and then opened the cubeMX file. I added one GPIO

out pin and saved/recompiled the CubeMX.

The Src and FATfs folders of the originator project were completely erased. There remains

a serious bug despite the partial fix that Pavel reported.

Does anyone know how to formally report this with ST?

Heiko

Pavel A.
February 20, 2020

Repeated generation in CubeMX is a separate issue, lets not mix them.

If we want the software to be cheap, even free - have to make concessions...

-- pa

KKane
KKaneAuthor
Associate II
February 21, 2020

Everytime setting again CubeMX .ioc manually to clone project is really painful...D:

And this issue never happend in True Studio...

gfe
Visitor II
April 30, 2020

renaming all references in .project, .cproject and .mxproject is still painful, but works for me and allows subsequent MX runs without deleting sources from the original project

inotec
Associate
March 16, 2021

I make 2 copies of the original folder. I use the first copy for the clone. When, as described above, the src is deleted from the original I delete the original and rename the 2nd copy back.

abbb.12
Associate
April 1, 2021

I had the same experience,and find why this happen。

�?CubeIDE】Why delete my Src folder ?Why haven't you fix it for so long?

inotec
Associate
April 1, 2021

Here's what I started doing: If I want to clone something from Project_01 folder, I just make a copy of the entire folder (in Windows, not in CubeMXIDE) and name it Project_02. All the project files within the folders will have identical names, so this might not work for everyone. Works great for me though. I just let the top folder describe the project.

JNguyen
Senior
May 12, 2021

I still have the same problems with copy a project in CubeIDE 1.6.0. This is simple primary task of CubeIDE. But it couldn't be done.

Cartu38 OpenDev
Graduate II
May 12, 2021

According to me issue has been found by @abbb.1​ see : �?CubeIDE】Why delete my Src folder ?Why haven't you fix it for so long? (st.com)

Trouble is .mxproject file.

Copy/paste from post shared above my proposal about how to clone :

Good finding ! Would help @STM_support.

Then I guess .mxproject is not useless .... Such is Device Configuration tool metadata. Removing them may leading to extra pain ... especialy if asking at a point to perform some project update if revisiting some IP setting or ... Such .metadata are kind of memory of project life history ... loosing it may have drawbacks.

Instead remove it maybe better to keep it but to rework it. I.e. doing project clone let's patch such file especialy updating absolute path ...

 

Myself always careful about hacking / removing metadata ... such are never useless and as end users we are not aware of they are serving product behavior ...

 

Another way to do being safer I guess is:

1) you're intending to clone your project so called "myProject1"

2) copy (Thanks favorite explorer or ...) your current project to "myProject1_temp"

3) Thanks IDE rename "myProject1" to "myProject2" .... please notice here project renaming is propagated to .ioc file name and content AND .mxproject file content

4) Back to your favorite explorer rename "myProject1" to "myProject2"

5) Back to your favorite explorer rename "myProject1_temp" to "myProject1"

6) Within IDE refresh project explorer (F5 key) and import "myProject1"

 

I may agree all such is not so user friendly but fact based neither Eclipse vanilla nor STM32CubeiDE promote project clone feature ...