Skip to main content
Associate III
Feb 11, 2025 11:06 AM UTC
Question

Issue raised in dual core debugging while adding images in the external sdram memory

Hii,

I am using STM32H745XIX6 microcontroller for our custom boards and also enabling the Touch GFX in it, we are doing dual core debugging, and the both the cores got activated and working fine after changing some settings in debug configurations of both the cores.

To check the dual core debugging, I have changed the debug configurations to "Connect under Reset" and selected "Halt all cores" in 1st Core (CM7) and changed the debug configurations to "None" in 2nd Core (CM4).

To add the images in the external SDRAM, I have added the external flash section in the flash linker script. Images that I have added in the Touch GFX are storing in the external SDRAM Memory. Then, I am getting problem in the debugging. What might be the issue?

If I've changed the debug configurations to "None" in 1st Core (CM7) then the debugging after changing the linker file is fine. But only 1st Core is going into debug.

Both the dual core debugging and when storing the Images in the external SDRAM Memory after changing the linker file are not working simultaneously (i.e. Issue in Debugging). I need to work on dual core debugging and also my images should store in the external SDRAM Memory.

Thank You...

 

 

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Feb 11, 2025 11:15 AM UTC

@Shivani wrote:

I am getting problem in the debugging.


What problem, exactly, are you getting?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ShivaniAuthor
Associate III
Feb 11, 2025 11:38 AM UTC

Hii @Andrew Neil ,

When adding the data in the external SDRAM Memory rather than Internal flash, I am getting debug issue as"Error in final launch sequence" 

Andrew Neil
Super User
Feb 11, 2025 12:19 PM UTC

Show the full log from the IDE console - copy & paste as text

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ShivaniAuthor
Associate III
Feb 11, 2025 12:27 PM UTC

STMicroelectronics ST-LINK GDB server. Version 7.8.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.17.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\SIGMAU~1\AppData\Local\Temp\STM32CubeProgrammer_a17852.log

ST-Link Server is running on port : 7184

ST-LINK SN : 67002900020000343132524E

ST-LINK FW : V2J45S7

Board : --

Voltage : 3.23V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x450

Revision ID : Rev V

Device name : STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7/M4

BL Version : 0x90

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a17852.srec

File : ST-LINK_GDB_server_a17852.srec

Size : 56.60 KB

Address : 0x08100000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sector 8

Download in Progress:

 

 

File download complete

Time elapsed during download operation: 00:00:01.554

 

 

 

Verifying ...

 

 

 

 

Download verified successfully

 

 

Shutting down...

Exit.