Is there STM32 Standalone Programmer which can flash the code without using a PC
Hello Everyone,
I am searching for a Standalone STM32 Programmer that can store the Program file inside it and can program the devices without the help of a PC.
we don't want to give the project file to the Production Team, so please suggest to us if there is any other way where we can protect our project file (HEX or BIN) from being misused.
We recently discovered the XStreamPro-Iso, which is a Standalone Programmer that can store HEX files in its memory and perform operations such as Chip protection. However, it supports many controllers like TI, Microchip, Atmel, STM32, etc., which makes it expensive. We're looking for an economical STM32 Dedicated Standalone Flash Programmer and would appreciate any suggestions you might have.
Thank you.