Skip to main content
johnvs2525
Associate
May 18, 2021
Question

Is there a way to stop STM32CubeIDE from collapsing the Project Explorer every time the project is built? This is an absolutely annoying "feature".

..

This topic has been closed for replies.

3 replies

TDK
May 19, 2021

Doesn't help you much, but it doesn't do so for me. I doubt it's intended. I'm on Win10, and have used many different IDE version.

"If you feel a post has answered your question, please click ""Accept as Solution""."
johnvs2525
Associate
May 19, 2021

If I have compilation errors that end the build process prematurely, mine doesn't do it either. Is it possible there is a project Properties setting that puts a command in the makefile that causes this action? I've looked around and can't find anything that looks like it would cause it.

johnvs2525
Associate
May 25, 2021

I finally figured this out. In the project Properties dialog, go to the "C/C++ Build" pane and the "Refresh Policy" tab. My project was listed. I deleted it from the list (it was the only thing listed) and no more post build "refreshing", i.e. completely collapsing every project folder I had open.

Thanks!