Skip to main content
DBURG.2449
Associate II
December 10, 2019
Question

Is there a newer version STM32CubeIDE for Mac OS?

When I try to install STM32CubeIDE on my MacBook Pro, I get a message following verification that the application is damaged.

I have re-downloaded several times with same result.

This topic has been closed for replies.

8 replies

Markus GIRDLAND
ST Employee
December 11, 2019

Exactly which error are we talking about here and when do you get it? Could you post a screenshot?

DBURG.2449
Associate II
December 12, 2019

The installation appears successful. Then, when I right click on the application, the system verifies the file instead of giving me the option to open the file as shown in the attached image. Then, the system reports that the file is damaged in should be trashed as shown in the second screen shot. Finally, I attach a screenshot showing the version of my operating system.

Markus GIRDLAND
ST Employee
December 12, 2019

Try the following command in the Terminal.app, you might have to prefix it with sudo:

$ xattr -cr /Applications/STM32CubeIDE.app

DBURG.2449
Associate II
December 12, 2019

OK, the IDE now starts, but when I try to start a new stm32 project, the stm32 target selector fails to download files and initialize. Refer to attached screen shot.

DBURG.2449
Associate II
December 12, 2019

first image showing verification:

DBURG.2449
Associate II
December 12, 2019

second image showing error message

Cartu38 OpenDev
Graduate II
January 10, 2020

Yes STM32CubeIDE 1.2.0 has been released some days ago. According release notes MacOS issues should be solved !