Skip to main content
November 14, 2021
Question

Is RTOS CMSIS_V2 working with USB Host?

Hello,

I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V2 and is not working with USB Host.

I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V1 and is working with USB Host.

Should I use CMSIS_V1 only?

Should CMSIS_V2 also work with USB Host?

This topic has been closed for replies.

3 replies

ST Technical Moderator
November 26, 2021

Hello @rtek1000​ ,

 What kind of error do you observed?

Do you face this issue when using CubeMx for project generation ?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
November 26, 2021

​Hello @Imen DAHMEN​ ,

​

Did not generate any Debug message for USB Host using RTOS CMSIS V2.

​

But for RTOS CMSIS V1 it generated the Debug messages normally.

​

I used the D.C.T.C. Generator from STM32CubeIDE ver. 1.7.0.

​

Thank you.​

Associate II
April 27, 2024

Hello  @Imen DAHMEN, @rtek1000​,

Any update on this as I am also facing the same issue.
I am using STM32Cube IDE v1.13 and stm32f746 discovery board, when I am using freeRTOS CMSIS-V1 USB host works very as a MSC host.

But as soon as I shift to CMSIS-V2  and connect the USB to the board the code gets stuck in the infinite loop of xTaskRemoveFromEventList().

 

But if I do not connect the USB the firmware's other functionalities are performing as intended.

Any inputs are highly appreciated.

Thankyou