Skip to main content
SElli.11
Associate III
September 9, 2019
Question

Is it still necessary to install ia32-libs and openjdk 8 when installing STM32CubeIDE on Kubuntu ?

Hi,

I have just downloaded and am about to install e.st-stm32cubeide_1.0.2_3566_20190716_0927_amd.deb_bundle.sh.zip onto Kubuntu 19.04.

As STM32CubeIDE seems to contain STM32CubeMX I was wondering if it was still necessary to install both openjdk 8 and ia32-libs prior to installing STM32CubeIDE.

The installation of openjdk 8 has proceeded without any problems.

However there seems to be a problem with the package ia32-libs. According to

https://askubuntu.com/questions/107230/what-happened-to-the-ia32-libs-package

the ia32-libs package seems to have been replaced with a Multi Arch package.

So, given that the ia32-libs package seems to still be available and in order to cater for any required 32-bit functionality, should I install the more up-to-date Multi Arch package or stick with the apparently deprecated ia32-libs package ?

Also, what other 32-bit packages would need to be installed if I install ia32-libs ?

Best regards,

Stuart

This topic has been closed for replies.