Is it possible to mix different amounts of colours in an RGB LED using HAL_GPIO_WritePin pinSet, as in WITHOUT using PWM?
I have a thermistor hooked up to the nucleo-l432kc to obtain temperature and display that temp on an LCD, print it to the screen, and light up a specific colour of an RGB LED. I want to be able to combine two colours of an RGB LED in different amounts, so not just have them both ON at full, but instead have one a bit less than the other (to make orange). I tried this using PWM and it worked, but for some reason it causes other parts of my circuit/program to malfunction (it ends up displaying an incorrect temp only when I use PWM and I do not know why). Any suggestions how to do this only using gpio outputs?