Skip to main content
Associate
Oct 6, 2023 9:16 AM UTC
Question

IOC tab not rendering in Ubuntu

I have a freshly installed stm32cubeide 1.13.2 on my ubuntu 22.04 machine and I've created a new workspace with a new project. In the beginning, everything works fine. But after generating code, closing the ioc file tab, closing the IDE and reopening the IDE with the same workspace and attempting to open the IOC file, it opens a blank tab failing to render the IOC file. If I close the tab and reopening it, the IDE hangs sometimes, or fails like before. It also seems to be using a whole lot of cpu resources. Reinstalling the IDE did not solve the problem.

This topic has been closed for replies.

15 replies

Ghofrane GSOURI
ST Technical Moderator
Oct 31, 2023 8:50 AM UTC

Hello @falconLucas 

First let me thank you for reporting.

This issue is reported internally (Internal ticket number:165338) .

I will keep you posted with updates.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Oct 31, 2023 1:09 PM UTC

I found only one solution after all. The CubeMX seems to be installed sepparately under home/STM32Cube/Repository. After manually deleting any versions newer than v1110, it came back to life. But the IDE updates it sometimes and the problem reappears. Hope this information may come useful.

Associate III
Dec 13, 2023 7:40 AM UTC

I've the same problem...

If can help, this is what I see running the IDE from cli:

claudio@claudio-i7:~$ /opt/st/stm32cubeide_1.12.1/stm32cubeide
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
1 : Invalid condition id : UX_CORESTACK_Condition cause : null
SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.
Nominal
Exception in thread "AWT-EventQueue-0" java.lang.StringIndexOutOfBoundsException: begin 0, end -1, length 18
at java.base/java.lang.String.checkBoundsBeginEnd(String.java:4606)
at java.base/java.lang.String.substring(String.java:2709)
at com.st.microxplorer.plugins.ip.adc.model.ADCParamManager.updateIpParameters(ADCParamManager.java:735)
at com.st.microxplorer.plugins.ipmanager.generictreatment.model.ParamManager.setConfigurationState(ParamManager.java:714)
at com.st.microxplorer.plugins.ipmanager.generictreatment.model.ParamManager.setConfigurationState(ParamManager.java:696)
at com.st.microxplorer.plugins.ip.adc.ADC.setConfigurationState(ADC.java:185)
at com.st.microxplorer.plugins.ipmanager.gui.IPsOverviews.setConfigState(IPsOverviews.java:2752)
at com.st.microxplorer.plugins.ipmanager.gui.BlockDiagram.updateIPConfigState(BlockDiagram.java:1557)
at com.st.microxplorer.plugins.ipmanager.gui.BlockDiagram.propertyChange(BlockDiagram.java:1269)
at java.desktop/java.beans.PropertyChangeSupport.fire(PropertyChangeSupport.java:343)
at java.desktop/java.beans.PropertyChangeSupport.firePropertyChange(PropertyChangeSupport.java:335)
at java.desktop/java.beans.PropertyChangeSupport.firePropertyChange(PropertyChangeSupport.java:268)
at com.st.microxplorer.util.MXPropertyChangeSupport.firePropertyChange(MXPropertyChangeSupport.java:54)
at com.st.microxplorer.mxsystem.MxSystem.MxFirePropertyChange(MxSystem.java:220)
at com.st.microxplorer.plugins.filemanager.engine.MainFileManager.userLoadConfig(MainFileManager.java:313)
at com.st.microxplorer.plugins.filemanager.FileManagerView.getSpecificTask(FileManagerView.java:247)
at com.st.stm32cube.common.mx.editor.CubeMxEditor.getMxTabbedPaneInstance(CubeMxEditor.java:1184)
at com.st.stm32cube.common.mx.editor.CubeMxEditor$12$1.createSwingComponent(CubeMxEditor.java:1065)
at com.st.stm32cube.common.mx.oss.core.awtswtbridge.EmbeddedSwingComposite.doComponentCreation(EmbeddedSwingComposite.java:492)
at com.st.stm32cube.common.mx.oss.core.awtswtbridge.EmbeddedSwingComposite$4.run(EmbeddedSwingComposite.java:291)
at com.st.stm32cube.common.mx.oss.core.awtswtbridge.AwtEnvironment$2.run(AwtEnvironment.java:166)
at java.desktop/java.awt.event.InvocationEvent.dispatch(InvocationEvent.java:318)
at java.desktop/java.awt.EventQueue.dispatchEventImpl(EventQueue.java:773)
at java.desktop/java.awt.EventQueue$4.run(EventQueue.java:720)
at java.desktop/java.awt.EventQueue$4.run(EventQueue.java:714)
at java.base/java.security.AccessController.doPrivileged(AccessController.java:399)
at java.base/java.security.ProtectionDomain$JavaSecurityAccessImpl.doIntersectionPrivilege(ProtectionDomain.java:86)
at java.desktop/java.awt.EventQueue.dispatchEvent(EventQueue.java:742)
at java.desktop/java.awt.EventDispatchThread.pumpOneEventForFilters(EventDispatchThread.java:203)
at java.desktop/java.awt.EventDispatchThread.pumpEventsForFilter(EventDispatchThread.java:124)
at java.desktop/java.awt.EventDispatchThread.pumpEventsForHierarchy(EventDispatchThread.java:113)
at java.desktop/java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:109)
at java.desktop/java.awt.EventDispatchThread.pumpEvents(EventDispatchThread.java:101)
at java.desktop/java.awt.EventDispatchThread.run(EventDispatchThread.java:90)

 

Associate II
Dec 13, 2023 8:25 AM UTC

Hello,

same issue here with STM32CubeIDE 1.14.0 and Ubuntu 23.10.

Each time I open the IDE, ioc tab is empty, the log is full of errors and I cannot even close the IDE by clicking the cross icon: it just does nothing and a popup says "not responding...". Almost unusable !!

I have found a tip to make things better : before launching the IDE, clean-up the following:

rm STM32CubeIDE/workspace_xxx/.metadata/.lock

rm -rf STM32CubeIDE/workspace_xxx/.metadata/.plugins

It does not solve the empty ioc tab issue but at least it avoids the IDE to crash or not respond...

Visitor II
May 25, 2024 7:52 PM UTC

I've got the same issue on STM32CubeIDE 1.15.1 and Ubuntu 24.04.4

Pavel A.
May 25, 2024 8:03 PM UTC

Will the cubeide behavior return to normal after reboot or session restart (aka logoff/logon)?

 

Visitor II
May 25, 2024 8:16 PM UTC

It was my first time running cubeide, it has not worked before. Also just reinstalled everything and still does not render.

Associate
May 27, 2024 4:15 PM UTC

I tried reinstalling the the IDE as well, as mentioned. But the problem clearly is not with the IDE, but with the related CubeMX software. So I'd call that the same symptoms as I had

Visitor II
May 29, 2024 11:18 PM UTC

My current work around is just to open the code and project in IDE but just the IOC file in CubeMX and it consistently works, albeit slowing down my workflow a bit.

Associate III
May 28, 2024 5:20 AM UTC

Hi, I use CUBEMX on ubuntu 22.04 pretty much every day. I understand the problems encountered and at the beginning I also felt a certain amount of frustration. After several attempts I understood that there is certainly some problem but it could be mitigated. My development method was therefore to version the IOC file and proceed step by step.
When a blocking problem occurred I restored the previous version and started again. I've been working this way for almost a year now and I have to say it's working well.
Also keep in mind that the IO file can be opened with a file editor and is easy to understand.
Hope this is helpful.

Explorer II
Sep 8, 2025 9:41 AM UTC

You might use x11 rather than wayland (change on login screen).

Other option is to run the CubeMX with x11 backend on wayland:

GDK_BACKEND=x11 /opt/st/stm32cubeide_1.18.1/stm32cubeide


Explorer
Nov 2, 2025 3:07 PM UTC

using GDK_BACKEND=x11 seems to solve the IOC rendering issue. But it very frequently causes the rest of the Eclipse UI to freeze, rendering it useless. Only thing that works is the menu and titlebar.