Skip to main content
XR.1
Senior
Mar 8, 2024 5:32 AM UTC
Question

IOC CubeIDE viewer doesn't render in Linux Mint

Sometimes it works, sometimes it doesn't.

When I try to open the IOC viewer either the IDE freezes or the view isn't rendered properly, as you can see below. This misbehavior breaks my working flow and makes me waste a lot of time. Any ideas?

Captura de pantalla de 2024-03-07 23-23-07.png

2 replies

Nov 4, 2025 11:46 AM UTC

I've met the issue as well, the solution is to use GPU to render the interface:

Right click on the STM32CubeIDE shortcut in apps menu -> Properties

Set "Use dedicated GPU if available" checkbox.

In my case the IOC interface started to render quick and reliable.  

XR.1
XR.1Author
Senior
Nov 4, 2025 9:38 PM UTC

Hi! Thank you for the tip, but I guess it doesn't work for me that I'm using Linux Mint. I couldn't find an option inside Eclipse to enable the use of the GPU.

 

And ironically, today I haven't been able to use the IOC. It's been running for 20 minutes or so and it can't be rendered (100% CPU Java's usage):

Captura de pantalla de 2025-11-04 14-49-08.png

This is a plugin's problem: after deleting some of them the IOC renders. There are sometimes when the full IDE refuses to start at all, and deleting the same plugins solves it. 

Later on I'll write a tutorial on this issue. Meanwhile, the IOC windows looks like this (after I've lost a lot of time, Thank you ST :(

Captura de pantalla de 2025-11-04 15-32-58.png