Skip to main content
Associate
Oct 21, 2025 4:59 PM UTC
Question

"Internal error: null argument" trying to copy from example selector

I find one example that helps me at the "example selector" . I can open, edit, and run it. if I want to copy it, I have this error. Does anyone know the solution? It creates the project, but the subfolders are not fully copied, like 80% are not there.

nala_ed70_0-1761065895615.png

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
Oct 22, 2025 3:25 PM UTC

Hello @nala_ed70 

Could you please try these steps:

- Copy the project directory (so that it is on same directory level, to avoid relative issues)
- Delete all eclipse dotted sub directories. Keep only .project and .cproject dot files.
- Edit the .project file and change only the project name there.
- Import the new project into CubeIDE and REFRESH.

 

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.