Skip to main content
xisco
Senior
Oct 12, 2025 11:44 AM UTC
Question

Installing new operating system, CubeIde fails (libncurses5 linux problem)

Hello,

Since I installed a new version of linux mint (22.2), I can't upload my programs to the MCU.

CubeIde show this error:

 

Could not determine GDB version using command: arm-none-eabi-gdb --version

arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory

 

Searching in my system, I found libncurses.so.6, not libncurses.so.5

 

I read in the forum that I need to install libncurses5, but is not present in my repositories.

 

I found a possible solution adding "universe" repositories

 

sudo add-apt-repository universe

sudo apt install libncurses5

 

but libncurses5 still missing

 

I found a post from Semer Cherni (ST Employee) that say that "The Linux Mint 22 is not supported by STM32CubeIDE"

This post was written on 2024-10-07 12:12 PM

 

Is the problem still active, or I need to go back to the old version?

 

Thanks

 

 

This topic has been closed for replies.

4 replies

Pavel A.
Oct 12, 2025 4:13 PM UTC

AFAIK you can find and install other arm-none-eabi-gdb version that does not have this defect (dependency on obsolete libncurses).   There was a post in this forum but I could not find it.

xisco
xiscoAuthor
Senior
Oct 13, 2025 10:26 PM UTC

Hello,

 

Thanks for posting. I haven't found one that's easy to install yet.

When I do, I'll let you know.

 

Regards

Ghofrane GSOURI
ST Technical Moderator
Oct 13, 2025 8:25 AM UTC

Hello @xisco 

Based on RN0114 - Rev 35 :STM32CubeIDE 1.19.0 is supported in the following OS 

• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 41
• macOS® 14 (Sonoma), macOS® 15 (Sequoia)
Note: Windows is a trademark of the Microsoft group of companies.
Linux® is a registered trademark of Linus Torvalds.
Ubuntu® is a registered trademark of Canonical Ltd.
Fedora® is a trademark of Red Hat, Inc.
macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions

Linux Mint 22.2 is not explicitly listed among the supported operating systems.

However, try to  install STM32CubeIDE 1.19.0 using deb_bundle installer, it should install automatically all needed libraries including libncurses5. 

THX

Ghofrane 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
xisco
xiscoAuthor
Senior
Oct 13, 2025 10:18 PM UTC

Hello, and thanks for your post

 

Unfortunately I have the same problem with both installers, Generic Linux and deb_bundle.

 

Regards