Installing CMSIS and CMSIS_DSP - missing files
Board H745ZI
I have installed ARM.CMSIS 5.8.0 and CMSIS-DSP 1.15.0 via the IOC>Software packs> and selected the components I want available under Select components. I have then enabled them under Middleware and software packs so CMSIS and CMSIS-DSP are both green and ticked. I have clicked the generate code icon and I can see ARM_CMSIS under Middlewares>Third_Party>ARM_CMSIS and under Middlewares>Third_Party>ARM_CMSIS>Source I can see a bunch of the source files for DSP functions. The weird thing is that a whole bunch of functions are missing. So if I clean the project (just to check the compiler can see all of the required files) I get a bunch of errors.
What I do not understand is STM32CUBEIDE is clearly looking in the correct place, it just seems not all the files have been copied over from the pack repository.
Can someone help?