Skip to main content
BGruc.1
Associate
April 14, 2020
Question

Install fails on Win10 32-bit operating system

..

This topic has been closed for replies.

8 replies

BGruc.1
BGruc.1Author
Associate
April 14, 2020

"This installer is for 64-bit system, your sstem is 32-bit"

So what to to ? I am forced to use Win10-32.

Pavel A.
April 14, 2020

Get a second PC with a decent operating system?

If your PC has 64-bit processor, you can install 64-bit Windows in a virtual machine.

-- pa

BGruc.1
BGruc.1Author
Associate
April 14, 2020

I am a li´l confused, I can´t find any requirements restricting to a 64bit system.

In addition, the installer´s name is indicating both win32 and win64 :

st-stm32cubeide_1.3.0_5720_20200220_1053_x86_64

A second PC is no option.

regards

BG

Pavel A.
April 14, 2020

> A second PC is no option.

Then, how about Keil MDK? It is 32 bit.

Piranha
Principal III
April 14, 2020

The "x86_64" is from x86-64. Welcome to the Eclipse - a tool built on a slow virtual platform for the sake of cross platform compatibility, yet not supporting 32-bit platforms. :D

Piranha
Principal III
April 26, 2020

This is an inappropriate comparison. The macOS and iOS are software only for a specific platforms of one company. Eclipse on the contrary is meant to be a cross-platform universal development tool.

BGruc.1
BGruc.1Author
Associate
April 15, 2020

Oh,nonoononono.

No Apple and NO linux.

But I made a decision. For testing the nucleo boards I can borrow a 64bit PC.

I´ll buy an used old 32bit PC for my old zilog z8encore stuff, which I have to support for next few years.

If STMCubeMX is not my style... well... the time is come to do so anyway.

Thank you all for fast answering, stay healthy and clean

regards

Bernhard