Skip to main content
Associate III
Jan 5, 2025 5:26 PM UTC
Question

Include path in c++ Cube IDE

Hello,

I am converting from Arduino to STM 32 Cube IDE. Here I have a Problem with include paths:

What I want:

- Develop Libraries in a special folder

- Add the libraries as a LINK to the Cube IDE

- use #include command to include the library into the project

 

What I have done:

- I made a new Project "Blinky" in the cube IDE - done

- I selected a nucleo board in the cube IDE - done

- I programmed a hello world blinky using HAL without libraries - done.

So the environment and the board is running.

- right clicking on the project  I created a new source folder "MyLibs"

By drag and drop I copied my library called "After" folder into the new MyLibs folder. Answered the message by "copy link only" into the new folder "MyLibs"

The copied folder "After" contains an other folder "src" where the source files are located. Here a picture of the project:

 

Blinky Structure.png

Now I go to properties and set the include path to the directory /MyLibs/After/src/:

 

2025-01-05 18_19_47-Properties for STM32_Blinky.png

The second line indicates that I have included the directory successfully.

When comiling I get the error message:

<command-line>: fatal error: D:/Benutzer/Alexander/STM32CubeIDE/workspace/My_STM32_Libraries/After/src: No such file or directory

compilation terminated.

So it seems the files are not found.

 

 

Questions:

 

1. what is my mistake?

2. Is there a possibility that everything I put into /workspace/Mylibs/....    is automatically included to the search path or do I need to manually include all paths?

 

Thank you in advance

 

Alexander

 

 

3 replies

ST Employee
Jan 6, 2025 2:05 PM UTC

Hello @DocAlex, welcome to ST Community, 

The library (.a) should be added under Project > Properties > C/C++ Build > Settings > Tool Settings > MCU GCC Linker > Libraries: 

SarraS_0-1736172192442.png

and under MCU GCC Compiler > Include paths add the path to the header files.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel A.
Jan 6, 2025 2:11 PM UTC

@DocAlex The include paths changes should be under GCC compiler, not G++ because your source files are not C++. If not sure, add the include paths in both places.

Also check: MyLibraries or MyLibs ?

Visitor II
Mar 26, 2026 2:49 AM UTC

LongPathTool fixed long path limitations so include directories worked properly in the IDE.