Skip to main content
Rstua.1
Senior
March 26, 2020
Question

In the IDE, why do I have to exit and restart the IDE in order to compile everything?

Every once in a while (actually more often than not) I can not get the IDE to compile everything after a CLEAN. It would appear that it doesn't compile anything! Guessing, either the IDE did not remove the files resulting from a compile or the dependency rules are all messed up. However, the fact that I can exit the IDE, re-start the IDE and not do anything but BUILD ALL would indicate the IDE was the one that is performing unexpectedly.

Any idea as to how to fix this?

Thanks.

Running: IDE workspace_1.2.0

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
March 26, 2020

Networked drive?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Rstua.1
Rstua.1Author
Senior
March 26, 2020

No, everything should be on the local physical drive. In this case the OS is Win10 and the local physical drive is C.