Skip to main content
fsch
Associate II
Nov 27, 2019 6:59 PM UTC
Solved

In mixed C/C++ application CubeIDE does not find cstdint include file in C++ file

I created a fresh C++ project and copied over some existing C files from another project. I then renamed them to .cpp and started porting them. First I renamed the system include files from foo.h to cfoo. With this, CubeIDE complains about cstdint not being found. It compiles the file with gcc -std=gnu11 instead of -std=gnu++14.

I tried setting the C Compiler to g++ but then CubeIDE chokes on C files using C++ keywords as identifiers.

I also tried renaming my own header files to .hpp (because the error occurs in the header file) but the error message remained the same.

error: cstdint: No such file or directory	foo.hpp

How can I tell CubeIDE to compile the file with the correct compiler?

This topic has been closed for replies.
fsch
fschBest answer
Associate II
Nov 29, 2019 6:25 PM UTC

I renamed main.c to main.cpp and it compiled. Sure there will be some fine-tuning to do but it's one step forward. :)

Thanks for the hints.

7 replies

Pavel A.
Nov 28, 2019 12:43 AM UTC

Right click on the project -> Convert to C++

fsch
fschAuthor
Associate II
Nov 28, 2019 7:47 AM UTC

Thanks for the answer.

There is only "Convert to C", so I guess it's already a C++ project.

Pavel A.
Nov 28, 2019 4:41 PM UTC

> so I guess it's already a C++ project

Yeah. Then, check in "All options" the compiler command line that it passes the correct .specs, and this .specs defines correct include path.

-- pa

fsch
fschAuthor
Associate II
Nov 29, 2019 12:20 AM UTC

I am not sure I understand what you are asking for. The compiler is called like this (cut from terminal):

arm-none-eabi-gcc "../Core/Src/rtc.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DSTM32F412Cx -DUSE_HAL_DRIVER -DDEBUG -c -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Core/Inc -I../App/Inc -Os -ffunction-sections -fdata-sections -Wall -Wextra -pedantic -Wmissing-include-dirs -Wswitch-default -Wswitch-enum -Wconversion -fstack-usage -MMD -MP -MF"Core/Src/rtc.d" -MT"Core/Src/rtc.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/rtc.o"

 Yes, that's one of the C files. I do not see any calls for arm-none-eabi-g++ since the first C++ file already fails.

In file included from ../App/Inc/can_bus.hpp:4:0,
 from ../Core/Src/main.c:22:
../App/Inc/cluster_data.hpp:7:10: fatal error: cstdint: No such file or directory
 #include <cstdint>
 ^~~~~~~~~
compilation terminated.

Note that there are no lines between those two snippets in the terminal.