Skip to main content
Visitor II
Dec 6, 2025 5:09 AM UTC
Question

Importing Example project: can't unzip Cube-F4 package 1283

I have tried to import example project, in that after selecting example and board then it tried to unzip the required F4 packages(stm32cube_fw_f4*) but 1280 is unzipped successfully but 1283 cant unzip this error remains what to do to solve this?

1 reply

Peter BENSCH
ST Technical Moderator
Dec 6, 2025 10:05 AM UTC

Welcome @Gokul_23, to the community?

It's simple: first unpack 1280, then the patch 1283. Both end up in the same directory.

The ZIP file ending in 0 is the basic version, the ZIP file ending in a number >0 is the patch.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.