Skip to main content
GJamo.1
Associate II
Jun 25, 2023 9:33 AM UTC
Solved

Implement error handling using Motor profiler API

Is there a Motor profiler API or any other tool that I can use to retrieve the error status from the ST Motor pilot programmatically? I'm interested in obtaining informations about the following errors:

GJamo1_0-1687685234853.png

If it's not available, I would appreciate any alternative recommendations or approaches to achieve this functionality within a code-based context.

    This topic has been closed for replies.
    GJamo.1
    GJamo.1Best answer
    Associate II
    Jun 25, 2023 7:34 PM UTC

    I had a thourough look on motor control sdk and I found this: 

     

     

     

    /**
     * @brief It returns a 16 bit fields containing information about faults
     * currently present.
     * \n\link Fault_generation_error_codes Returned error codes are listed here \endlink
     * pHandle Pointer on the component instance to work on.
     * @retval uint16_t 16 bit fields with information about about currently
     * present faults.
     * \n\link Fault_generation_error_codes Returned error codes are listed here \endlink
     */
    __weak uint16_t MCI_GetCurrentFaults(MCI_Handle_t *pHandle)
    {
     return ((uint16_t)pHandle->CurrentFaults);
    }

     

    With the following error codes:

    /** 
     * @anchor fault_codes 
     * @name Fault codes
     * The symbols below define the codes associated to the faults that the 
     * Motor Control subsystem can raise.
     * @{ */
    #define MC_NO_ERROR ((uint16_t)0x0000) /**< @brief No error.*/
    #define MC_NO_FAULTS ((uint16_t)0x0000) /**< @brief No error.*/
    #define MC_DURATION ((uint16_t)0x0001) /**< @brief Error: FOC rate to high.*/
    #define MC_OVER_VOLT ((uint16_t)0x0002) /**< @brief Error: Software over voltage.*/
    #define MC_UNDER_VOLT ((uint16_t)0x0004) /**< @brief Error: Software under voltage.*/
    #define MC_OVER_TEMP ((uint16_t)0x0008) /**< @brief Error: Software over temperature.*/
    #define MC_START_UP ((uint16_t)0x0010) /**< @brief Error: Startup failed.*/
    #define MC_SPEED_FDBK ((uint16_t)0x0020) /**< @brief Error: Speed feedback.*/
    #define MC_BREAK_IN ((uint16_t)0x0040) /**< @brief Error: Emergency input (Over current).*/
    #define MC_SW_ERROR ((uint16_t)0x0080) /**< @brief Software Error.*/
    /** @}*/

    1 reply

    GJamo.1
    GJamo.1AuthorBest answer
    Associate II
    Jun 25, 2023 7:34 PM UTC

    I had a thourough look on motor control sdk and I found this: 

     

     

     

    /**
     * @brief It returns a 16 bit fields containing information about faults
     * currently present.
     * \n\link Fault_generation_error_codes Returned error codes are listed here \endlink
     * pHandle Pointer on the component instance to work on.
     * @retval uint16_t 16 bit fields with information about about currently
     * present faults.
     * \n\link Fault_generation_error_codes Returned error codes are listed here \endlink
     */
    __weak uint16_t MCI_GetCurrentFaults(MCI_Handle_t *pHandle)
    {
     return ((uint16_t)pHandle->CurrentFaults);
    }

     

    With the following error codes:

    /** 
     * @anchor fault_codes 
     * @name Fault codes
     * The symbols below define the codes associated to the faults that the 
     * Motor Control subsystem can raise.
     * @{ */
    #define MC_NO_ERROR ((uint16_t)0x0000) /**< @brief No error.*/
    #define MC_NO_FAULTS ((uint16_t)0x0000) /**< @brief No error.*/
    #define MC_DURATION ((uint16_t)0x0001) /**< @brief Error: FOC rate to high.*/
    #define MC_OVER_VOLT ((uint16_t)0x0002) /**< @brief Error: Software over voltage.*/
    #define MC_UNDER_VOLT ((uint16_t)0x0004) /**< @brief Error: Software under voltage.*/
    #define MC_OVER_TEMP ((uint16_t)0x0008) /**< @brief Error: Software over temperature.*/
    #define MC_START_UP ((uint16_t)0x0010) /**< @brief Error: Startup failed.*/
    #define MC_SPEED_FDBK ((uint16_t)0x0020) /**< @brief Error: Speed feedback.*/
    #define MC_BREAK_IN ((uint16_t)0x0040) /**< @brief Error: Emergency input (Over current).*/
    #define MC_SW_ERROR ((uint16_t)0x0080) /**< @brief Software Error.*/
    /** @}*/