Associate
Feb 18, 2025 5:58 AM UTC
Question
Impact of Clock Stretching and Applicability of Slave Features in STM32CubeIDE
- 1 reply
- 480 views
I am using the STM32F413VHT6 board and configuring I2C in STM32CubeIDE with STM32 as a master. I have the following questions regarding the Clock Stretching feature and Slave Features settings in the IDE:
- If I enable or disable Clock Stretching (listed under Slave Features), will it cause issues or improve my master communication?
- In STM32CubeIDE, are the Slave Features settings only applicable when STM32 is configured as a slave? Or can I still modify them when STM32 is in master mode, and will they have any effect?
I would appreciate any clarification on these points