If possible, how do you change the pin mapping of auto-generated code in STM32Cube?
I'm wanting to create a project for the Murata LoRa typABZ module, which appears to use the STM32L082CZU with UFQFPN48 package. In the IDE, I get the message: "The target device 'STM32L082CZUx' is currently not supported by STM32CubeIDE". I started a project using STM32L082CZY, but the pin mapping is different and somethings are not working. I don't see where, but can I change this mapping or is it more complicated than that? Or, is there a another way to auto-generate for this part? Will this be supported in the near future?