Skip to main content
Associate
Dec 8, 2025 3:16 PM UTC
Solved

IDE Version 2.0.0 - why remove MX ?

Why, oh why have you separated IDE and MX such that .ioc files can no longer be opened in IDE?

I cannot imagine any benefits and it makes the IDE significantly worse, such that I've felt compelled to revert to version 1.19.0 ( go to Help -> About STM32CubeIDE -> Installation Details -> Installation History -> select version -> Revert)

I couldn't find any other means of feeding back my strong dislike of this change other than a post like this. I hope version 2.1.0 comes out soon and re-integrates MX and IDE!

mattias norlander
ST Technical Moderator
Dec 8, 2025 5:55 PM UTC

Hi,

 

The main reason is the cost this integration brings inside our organization. MX is released 3 times per year in-sync with silicon launches. But, internally, a new version of MX is integrated into CubeIDE every week. Every week end-to-end test campaigns are executed to validate the progress of upcoming STM32 product launches. Amazing amount of R&D-hours are spent on just integrating and validating MX+IDE.

The end-users benefits from this integration are mainly: Download a single tools and no need to ALT-TAB between MX and IDE. 

Meanwhile the integration brings cost and risks:

  • Mixing apples and pears: Over time most STM32 developers learns that working with stand-alone MX and IDE is a good insurance to mitigate  tool related update risks and thereby frustration and project delays. Have a look at the CubeMX release history, many patch releases has been provided to fix code generation issues. The IDE features are rarely suffering from regressions. The IDE release cycle is completely hostage to MX.
  • MCU roadmap: ST has an aggressive MCU roadmap ahead of us. Tightly integrated tools like CubeIDE 1.X in combination with aggressive MCU roadmap is both a huge risk. Due to MX integration there is a real risk that CubeIDE is not ready in-time for an STM32 product launch. In any other IDE, target support is the simple part.
  • Integration cost: All R&D-effort spent on integration/validation could have been spent on feature and bug fixes.
  • 2x IDEs: Developers are more and more asking for VS Code and we need to split our R&D-bandwidth across two IDEs (Eclipse + VS Code).
  • Technical risks: The integration of Java/Swing and Java/SWT has been an exciting journey full of GUI surprises across our releases. Unclear how long this integration bridge will be maintained (not under ST control).

 

We have spoken to many customers in-advance of splitting these tools. Both small and large companies. The split is a bit more appealing to larger companies, and a bit less to small companies and beginners. IAR, Keil, VS Code, and CLion users are already exercising these workflows. And many CubeIDE users already realized that using MX and IDE in stand-alone mode allow them individual tool updates/freeze providing a good "risk approach" towards STM32 development.

The saved R&D bandwidth can help us secure that we can offer 2x IDEs in-sync with new STM32 product launches. Hopefully we can even fix a bug or two in the category of edit/compile/debug. That would be cool!

If I am correctly informed, CubeMX 6.16.0 contained some code generation bugs. Therefore, a bug fix release of MX will follow. In the integrated CubeIDE 1.X world, this would have forced a re-integration, re-validation and re-delivery of CubeIDE as well. Causing ST R&D-team a few weeks of delays or lost focus. Which could have been spent on real value-add! By splitting the tools we will hopefully not have to provide a patch release on CubeIDE as a consequence of CubeMX issues. That would be an amazing long-term win! ;)

 

We are not aiming to re-integrate CubeMX into CubeIDE.
We must get back on the track where our R&D-dollars are spent on tool innovation, not tool maintenance. 
We understand that this will hurt some developers, and for this we are sorry! The "interoperability journey" between stand-alone tools can still be improved.

 

Kind regards, Mattias

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

57 replies

Visitor II
May 17, 2026 6:32 AM UTC

Dear ST,

You were known as a standalone provider in the industry that offered a single tool (until STM32CubeIDE 1.9.0) capable of handling MCU configuration, IDE functionality, debugging, and everything else in one place. Developers chose your platform because of its simple and easy-to-use development environment.

Sorry to say this, but the development environment now feels unnecessarily fragmented. Separating the tools, confusing users, and making the setup process more complicated has taken away the simplicity that developers appreciated. We are now forced to spend time debugging the environment setup itself, similar to experiences with other suppliers.

You really need to reconsider these changes and bring back the simplicity that made STM32 development so popular. Otherwise, you risk losing the trust and appreciation you built with developers over the years.

Please rethink this before it is too late.

Pavel A.
May 17, 2026 8:27 AM UTC

@samsio_innovations  CubeIDE branch 1.x, with integrated MX still is available and supports majority of STM32 products. Just keep using it?

 

Visitor II
May 21, 2026 8:10 AM UTC

Hello Mattias,

Yes, I've replied to you. 

Thanks for your concern. 

AScha.3
Super User
May 23, 2026 9:34 AM UTC

STM just adheres to Murphy's Law.

 

  1. Any given program, when running, is obsolete.
  2. If a program is useful, it will have to be changed.
  3. After months of training and you finally understand all of a program's commands, a revised version of the program arrives with an all-new command structure.
If you feel a post has answered your question, please click on " Best Answer ".