Skip to main content
Associate III
October 31, 2023
Question

IAP issue with single bank flash

Hello experts,

I am using stm32f779I - EVAL evaluation kit, am trying to implement LWIP IAP on this board for that I have used example code from the repository C:\Users\Aravind\STM32Cube\Repository\STM32Cube_FW_F7_V1.17.0\Projects\STM32F769I_EVAL\Applications\LwIP\LwIP_IAP and binary file of application availabe in same repository, it is working fine as the binary file says four LEDS toggles, it is toggling.

 I have written my own application with flash base address 0x08020000 and vector offset = 0x20000 and loaded the binary file and tried to run  it is getting into not valid stack address (LED 3 is getting on ). I have attached the IAP code below which is working fine with binary file from repository but same IAP is getting into not valid stack address with my binary file.

if (((*(__IO uint32_t*)USER_FLASH_FIRST_PAGE_ADDRESS) & 0x2FFE0000 ) == 0x20000000)
{
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (USER_FLASH_FIRST_PAGE_ADDRESS + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) USER_FLASH_FIRST_PAGE_ADDRESS);
Jump_To_Application();
/* do nothing */
while(1);
}
else
{/* Otherwise, do nothing */
/* LED3 (RED) ON to indicate bad software (when not valid stack address) */
BSP_LED_Init(LED3);
BSP_LED_On(LED3);
/* do nothing */
while(1);
}

Please let me know what am I missing.

Thanks & Regards

Srikanth R.

 

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
October 31, 2023

If your Initial SP is valid and in RAM, fix the test so if passes. The test is relatively crude. An SP of 0x2001fff0 should pass. If you have more than 128KB adjust the test. Or adjust the SP in the Linker Script.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Srikanth1Author
Associate III
November 3, 2023

Hello Tesla DeLorean,

Thanks for the response.

I am attaching my linker file below can you please explain me particularly where I need to do changes,

/* Entry Point */

ENTRY(Reset_Handler)

 

/* Highest address of the user mode stack */

_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

 

_Min_Heap_Size = 0x2000; /* required amount of heap */

_Min_Stack_Size = 0x4000; /* required amount of stack */

 

/* Memories definition */

MEMORY

{

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K

FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 1024K

Memory_B1(xrw) : ORIGIN = 0x2007C000, LENGTH = 0xA0

Memory_B2(xrw) : ORIGIN = 0x2007C0A0, LENGTH = 0xA0

}

 

/* Sections */

SECTIONS

{

/* The startup code into "FLASH" Rom type memory */

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(4);

} >FLASH

 

/* The program code and other data into "FLASH" Rom type memory */

.text :

{

. = ALIGN(4);

*(.text) /* .text sections (code) */

*(.text*) /* .text* sections (code) */

*(.glue_7) /* glue arm to thumb code */

*(.glue_7t) /* glue thumb to arm code */

*(.eh_frame)

 

KEEP (*(.init))

KEEP (*(.fini))

 

. = ALIGN(4);

_etext = .; /* define a global symbols at end of code */

} >FLASH

 

/* Constant data into "FLASH" Rom type memory */

.rodata :

{

. = ALIGN(4);

*(.rodata) /* .rodata sections (constants, strings, etc.) */

*(.rodata*) /* .rodata* sections (constants, strings, etc.) */

. = ALIGN(4);

} >FLASH

 

.ARM.extab : {

. = ALIGN(4);

*(.ARM.extab* .gnu.linkonce.armextab.*)

. = ALIGN(4);

} >FLASH

 

.ARM : {

. = ALIGN(4);

__exidx_start = .;

*(.ARM.exidx*)

__exidx_end = .;

. = ALIGN(4);

} >FLASH

 

.preinit_array :

{

. = ALIGN(4);

PROVIDE_HIDDEN (__preinit_array_start = .);

KEEP (*(.preinit_array*))

PROVIDE_HIDDEN (__preinit_array_end = .);

. = ALIGN(4);

} >FLASH

 

.init_array :

{

. = ALIGN(4);

PROVIDE_HIDDEN (__init_array_start = .);

KEEP (*(SORT(.init_array.*)))

KEEP (*(.init_array*))

PROVIDE_HIDDEN (__init_array_end = .);

. = ALIGN(4);

} >FLASH

 

.fini_array :

{

. = ALIGN(4);

PROVIDE_HIDDEN (__fini_array_start = .);

KEEP (*(SORT(.fini_array.*)))

KEEP (*(.fini_array*))

PROVIDE_HIDDEN (__fini_array_end = .);

. = ALIGN(4);

} >FLASH

 

/* Used by the startup to initialize data */

_sidata = LOADADDR(.data);

 

/* Initialized data sections into "RAM" Ram type memory */

.data :

{

. = ALIGN(4);

_sdata = .; /* create a global symbol at data start */

*(.data) /* .data sections */

*(.data*) /* .data* sections */

*(.RamFunc) /* .RamFunc sections */

*(.RamFunc*) /* .RamFunc* sections */

 

. = ALIGN(4);

_edata = .; /* define a global symbol at data end */

 

} >RAM AT> FLASH

 

/* Uninitialized data section into "RAM" Ram type memory */

. = ALIGN(4);

.bss :

{

/* This is used by the startup in order to initialize the .bss section */

_sbss = .; /* define a global symbol at bss start */

__bss_start__ = _sbss;

*(.bss)

*(.bss*)

*(COMMON)

 

. = ALIGN(4);

_ebss = .; /* define a global symbol at bss end */

__bss_end__ = _ebss;

} >RAM

 

/* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */

._user_heap_stack :

{

. = ALIGN(8);

PROVIDE ( end = . );

PROVIDE ( _end = . );

. = . + _Min_Heap_Size;

. = . + _Min_Stack_Size;

. = ALIGN(8);

} >RAM

 

/* Remove information from the compiler libraries */

/DISCARD/ :

{

libc.a ( * )

libm.a ( * )

libgcc.a ( * )

}

 

.ARM.attributes 0 : { *(.ARM.attributes) }

.RxDecripSection (NOLOAD) : { *(.RxDecripSection) } >Memory_B1

.TxDecripSection (NOLOAD) : { *(.TxDecripSection) } >Memory_B2

}

Thanks & Regards

srikanth R