Skip to main content
VPing.1
Associate
Dec 24, 2020 8:13 AM UTC
Solved

Iam using STM32F072B-DISCO board with STM32Cube IDE and FreeRTOS. But, i have no idea how to send/receive data from mini USB ports in it. Can somebody help with it?

..

This topic has been closed for replies.
Mazen Aljeddani
Mazen AljeddaniBest answer
Visitor II
Dec 25, 2020 4:22 PM UTC

Hi VPing.1,

The easiest way, is to configure the mini USB as VCP(Virtual Comm Port).

So, you can use it as serial interface (UART) from Micro Controller Side.

From the PC side, will be as serial comm port.

https://www.youtube.com/watch?v=AYICE0gU-Sg

Regards,

Mazen

5 replies

Ons KOOLI
Visitor II
Dec 25, 2020 10:39 AM UTC

Hi VPing.1,

To start with USB please refer to our STM32 USB trainings.

You can also find ready USB developed applications in the STM32CubeF0 under \Projects\STM32F072B-Discovery\Applications.

Best Regards,

Ons.

VPing.1
VPing.1Author
Associate
Dec 26, 2020 10:21 PM UTC

Hello Ons,

Thanks for reply. Its long way to go. Parallely checking. STM32F072B with STM32CubeIDE videos would be more helpful. Also, i cannot see USB device at all detected in "ls tty" . Can see device in "lsusb" when connected USB-STLink. But, cannot see device in "lsusb" when connected "USB User" only . I might be missing something here. Any further help appreciated.

Thanks&Regards

Vinay

Mazen Aljeddani
Mazen AljeddaniBest answer
Visitor II
Dec 25, 2020 4:22 PM UTC

Hi VPing.1,

The easiest way, is to configure the mini USB as VCP(Virtual Comm Port).

So, you can use it as serial interface (UART) from Micro Controller Side.

From the PC side, will be as serial comm port.

https://www.youtube.com/watch?v=AYICE0gU-Sg

Regards,

Mazen

VPing.1
VPing.1Author
Associate
Dec 26, 2020 10:17 PM UTC

Hello Mazen,

Thanks for quick reply. I understand that CUBE IDE contains CUBE MX . So, CUBE IDE generates code and I'm able to compile and download to device. But, cannot find similar APIs as in video with CUBE MX. Am i missing some knowledge here? Even i cannot see any tty devices in Ubuntu. Sorry, i'm new to this STM open source world.

Further help greatly appreciated.

Thanks&Regards

Vinay