Skip to main content
HAhme.1
Associate II
October 2, 2020
Question

I2c in different versions of STM32CubeIDE does not work as should.

Hello,

I have an old project which is on an older version of STCubeMX firmware, and once I migrate it to the new firmware, it stops communicating with the I2C correctly. Is there a reason for this? And how can I possibly fix this?

I'm using the STM32L4RET chip and I've attached the pop up message that comes up to me when I migrate.0693W000004IXLnQAO.jpg

This topic has been closed for replies.

4 replies

TDK
October 2, 2020

It's most likely a bug with CubeMX or the code generation process. I would diff the main.c file before/after the migration, and if that doesn't lead to relevant differences, other files.

"If you feel a post has answered your question, please click ""Accept as Solution""."
HAhme.1
HAhme.1Author
Associate II
October 2, 2020

I'm doing that right now, but it's a bit long and tedious. Is there no other way because I'm facing a deadline.

Thanks!

TDK
October 2, 2020
You could pay someone else to do it. You could write your own code so you're not restricted to what CubeMX outputs. You could avoid upgrading/migrating to newer versions unless absolutely needed, and plan for some time to find and fix issues that arise.
"If you feel a post has answered your question, please click ""Accept as Solution""."
October 2, 2020

Maybe that's the price of updating the build tool during the development of the project, I already noticed this type of problem with Ethernet and USB Host.