Skip to main content
CMcC.1
Associate III
September 18, 2021
Question

I keep on running into -> void HardFault_Handler(void); When my HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *) pwmData, index); Is called

Hi. I seem to get HardFault_Handler error when I start my HAL_TIM_PWM_start_DMA function.

I am not sure if it just gets stuck in an infinite loop in the while() called right after it.

This looks like allot of code but really its just 5 of my functions including main().

My TIM1 is set to Internal Clock and its on PWM Generator CH1 with Counter Period set to (80-1).

What could possibly be the reason for the HarFault?

-------------------------------------------------------------*/
#include "main.h"
 
--------------------------------------------------*/
TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_ch1;
 
---------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM1_Init(void);
 
#define MAX_LED 8
#define USE_BRIGHTNESS 1
 
uint8_t LED_Data[MAX_LED][4];
uint8_t LED_Mod[MAX_LED][4];
 
int data_sent_flag = 0;
 
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef * htim){
	HAL_TIM_PWM_Stop_DMA(&htim, TIM_CHANNEL_1);
	data_sent_flag = 1;
}
 
void Set_LED(int LEDNum, int Red, int Green, int Blue){
	LED_Data[LEDNum][0] = LEDNum;
	LED_Data[LEDNum][1] = Green;
	LED_Data[LEDNum][2] = Red;
	LED_Data[LEDNum][3] = Blue;
 
}
 
void Set_Brightness(int brightness){
	if (brightness > 45) {brightness = 45;}
	for (int i=0; i<= MAX_LED; i++){
		LED_Mod[i][0] = LED_Data[i][0];
		for(int j=1; j<4; j++){
			LED_Mod[i][j] = 90 - brightness;
		}
	}
};
 
uint16_t pwmData[(24*MAX_LED)+50];
 
void WS2812_Send(void){
	uint32_t index=0;
	uint32_t color;
 
 
	for (int x = 0 ; x < MAX_LED ; x++){
		color = ( (LED_Mod[x][1]<<16 | (LED_Mod[x][2]<<8) | (LED_Mod[x][3]) ) );
 
		for(int y = 23; y >=0 ; y--){
			if(color&(1<<y)){
				pwmData[index] = 60;
			} else {
				pwmData[index] = 30;
			}
 
			index++;
		}
	}
 
	for(int o = 0 ; o < 50 ; o++){
		pwmData[index] = 0;
		index++;
	}
 
	HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *) pwmData, index);
	while(!data_sent_flag){};
	data_sent_flag = 0;
}
 
int main(void)
{
 
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM1_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 Set_LED(0, 255, 0, 0);
 Set_LED(1,0,255,0);
 Set_LED(2,0,0,255);
 Set_Brightness(45);
 WS2812_Send();
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_6);
	 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
 /** Configure the main internal regulator output voltage 
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
 RCC_OscInitStruct.PLL.PLLN = 8;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the peripherals clocks 
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_TIM1;
 PeriphClkInit.Tim1ClockSelection = RCC_TIM1CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief TIM1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM1_Init(void)
{
 
 /* USER CODE BEGIN TIM1_Init 0 */
 
 /* USER CODE END TIM1_Init 0 */
 
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
 /* USER CODE BEGIN TIM1_Init 1 */
 
 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 80-1;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_OC_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_OC_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */
 
 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);
 
}
 
/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_6, GPIO_PIN_SET);
 
 /*Configure GPIO pin : PC6 */
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
}
 
void Error_Handler(void)
{
}
 
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{ 
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This topic has been closed for replies.

3 replies

TDK
September 18, 2021

> uint8_t LED_Data[MAX_LED][4];

> uint8_t LED_Mod[MAX_LED][4];

> for (int i=0; i<= MAX_LED; i++){

> LED_Mod[i][0] = LED_Data[i][0];

> for(int j=1; j<4; j++){

> LED_Mod[i][j] = 90 - brightness;

> }

> }

Looks like you're writing to out of bounds arrays. Indices are 0-based in C.

Could be other issues. Look at SCB registers for the reason behind the hard fault.

Why don't you know if it's in a hard fault or in a while loop? Where is execution when you debug and pause the program?

"If you feel a post has answered your question, please click ""Accept as Solution""."
CMcC.1
CMcC.1Author
Associate III
September 19, 2021

@TDK​ Ok so I got it to not throw the void HardFault_Handler(void);

But now that I run the DMA in the while loop it crashes the second time.

Sometimes when I just run the code it can not talk to the debugger. When I comment that code that runs WS2812_Send() it runs fine and actually toggles the led_PC6.

I have added the new code.

#include "main.h"
 
TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_ch1;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM1_Init(void);
 
#define MAX_LED 8
#define USE_BRIGHTNESS 1
 
uint8_t LED_Data[MAX_LED][4];
uint8_t LED_Mod[MAX_LED][4];
 
int data_sent_flag = 0;
 
 
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
	HAL_TIM_PWM_Stop_DMA(&htim1, TIM_CHANNEL_1);
	data_sent_flag=1;
}
void Set_LED (int LEDnum, int Red, int Green, int Blue)
{
	LED_Data[LEDnum][0] = LEDnum;
	LED_Data[LEDnum][1] = Green;
	LED_Data[LEDnum][2] = Red;
	LED_Data[LEDnum][3] = Blue;
}
 
void Set_Brightness (int brightness) // 0-45
{
 
	if (brightness > 45) brightness = 45;
	for (int i=0; i<MAX_LED; i++)
	{
		LED_Mod[i][0] = LED_Data[i][0];
		for (int j=1; j<4; j++)
		{
			LED_Mod[i][j] = brightness;
		}
	}
 
}
uint16_t pwmData[(24*MAX_LED)+50];
 
void WS2812_Send (void)
{
	uint32_t indx=0;
	uint32_t color;
 
 
	for (int i= 0; i<MAX_LED; i++)
	{
		color = ((LED_Mod[i][1]<<16) | (LED_Mod[i][2]<<8) | (LED_Mod[i][3]));
 
 
		for (int i=23; i>=0; i--)
		{
			if (color&(1<<i))
			{
				pwmData[indx] = 60; // 2/3 of 90
			}
 
			else pwmData[indx] = 30; // 1/3 of 90
 
			indx++;
		}
 
	}
 
	for (int i=0; i<50; i++)
	{
		pwmData[indx] = 0;
		indx++;
	}
 
	HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)pwmData, indx);
	while (!data_sent_flag){};
	data_sent_flag = 0;
}
 
int main(void)
{
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM1_Init();
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 Set_LED(0, 255, 0, 0);
 Set_LED(1,0,255,0);
 Set_LED(2,0,0,255);
 Set_LED(3,0,0,255);
 Set_Brightness(8);
 WS2812_Send();
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 uint8_t X = 5;
 int8_t flip = 0;
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_6);
	 HAL_Delay(1000);
	 if (X == 4){
		 Set_Brightness(30);
		 WS2812_Send();
	 }
	 X++;
	 //WS2812_Send();
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
 RCC_OscInitStruct.PLL.PLLN = 8;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_TIM1;
 PeriphClkInit.Tim1ClockSelection = RCC_TIM1CLKSOURCE_PCLK1;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}
 
static void MX_TIM1_Init(void)
{
 
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 80-1;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_TIM_MspPostInit(&htim1);
 
}
 
static void MX_DMA_Init(void) 
{
 
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 
}
 
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_6, GPIO_PIN_SET);
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
}
 
void Error_Handler(void)
{
}
 
#ifdef USE_FULL_ASSERT
 
void assert_failed(uint8_t *file, uint32_t line)
{ 
}
#endif 

TDK
September 20, 2021

Define "crashes". When you debug the program, where is execution?

data_sent_flag should be volatile.

"If you feel a post has answered your question, please click ""Accept as Solution""."