Skip to main content
Catutigernos
Associate II
March 17, 2024
Question

I can not activate the Ethernet

Hi everyone,

I have a NUCLEO-H745ZI-Q board. I try to activate ethernet, but I could not. I watched videos, read tutorials, post about it. Firstly, I thought it was my mistake. I must have made a mistake somehere, so I downloaded stm32 ethernet example for the board (NUCLEO-H745), built it, uploaded it, and it is not working too. How can I solve this problem?

Thanks in advance. 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
March 17, 2024

Hello @Catutigernos 

You can find a simple Ethernet examples based on LwIP and FreeRTOS, running on Nucleo-H745zi-q board here:

Also, ensure that there is no restrictions on the Ethernet network that you are using (for security or other restrictions).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Catutigernos
Associate II
March 18, 2024

Hi @STTwo-32,
Thanks for your response. I already tried these examples, they are not working for me. Ethernet cable was directly connected to the computer. I configured my network settings to be on the same network with the board(no ip address conflicts). There is no any other network with same ip address range. I checked the firewall settings there is no any problems for that. I connect a plc which is set same address with the board, I connect the plc ethernet port directly to my computer ethernet port with ethernet cable and they communicate easily, but I could not same thing with the board.