Skip to main content
PDutt.2
Associate II
December 24, 2020
Question

I am following the course "STM32L4 workshop". The course uses STM32L476G-DISCO board and I am having STM32L475 Discover Kit IoT Node (B-L475EIOT01A2C). What changes needed in the example code to make it working.

I also checked directly using binary files provided, but there is no output on the COM port. I tried to compile and run using IAR Embedded Workbench, there is no error, only following message which is worth mentioning:

"C:\GCP\STM32L4_Workshop_V1.5\HandsOn\1_System_Operating_Modes\1_RUNMODE\EWARM\STM32L476(FLASH)\Exe\RUNMODE Configuration.out to flash memory."

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
December 24, 2020

When porting code between boards you're going to need to pay attention to pin differences, especially those of the USART/VCP. With GPIOG bank pay particular attention to the VCCIO enable.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PDutt.2
PDutt.2Author
Associate II
December 24, 2020

Thanks for the suggestion. I shall try to locate the pin differences or I shall create a totally new project and just use the functionalities of main c file for testing.