I am facing some bug issue in stm32cubeide.
Dear Sir,
I am working in STM32CUBEIDE,In that i am working with ST-LINK OPEN OCD.Previously it works in good manner without
any issues but now i am facing some error regarding BUG ISSUE.I delete and reinstall the software also. I have mentioned
that errors below ,kindly plz rectify my queries asap.
Regards & thanks,
IYYANAR.K
Open On-Chip Debugger 0.10.0+dev-01288-g7491fb4 (2020-10-27-17:36)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.161807
Error: init mode failed (unable to connect to the target)
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:3333
Error message from debugger back end:
localhost:3333: The system tried to join a drive to a directory on a joined drive.
Failed to execute MI command:
target remote localhost:3333
Error message from debugger back end:
localhost:3333: The system tried to join a drive to a directory on a joined drive.
localhost:3333: The system tried to join a drive to a directory on a joined drive.