Skip to main content
JLivn
Associate
Aug 14, 2019 5:57 PM UTC
Solved

I am doing my first attempt with STM32CubeIDE (Ver 1.0.2) and after selecting the MCU model and naming the project, I get a message "Create minimal project failure: Cannot read template source". Please direct me.

..

This topic has been closed for replies.
kris2399
kris2399Best answer
Associate II
Sep 30, 2020 2:12 PM UTC
Hi Mattias,
Thanks for your reply. I’ve been I’m using the AC6 toolchain and Eclipse. There seems tob e a known issue which relates to his kind of issues: see https://bugs.eclipse.org/bugs/show_bug.cgi?id=67719
In accordance to this bug report I added the lines (Note the line “-Djava… “ didn’t dot he trick)
-Djava.io.tmpdir=c:\STM32Dev\tmpdir
-configuration c:\STM32Dev\tmpdir
In my eclipse.ini file
Now it seems fine: I also see the .tmp file in the directory specified by the -configuration (whereas it was previously written to de default directory)
Maybe this can help other people,
Thanks again for putting me on this track,
Kris Demets

21 replies

mattias norlander
ST Technical Moderator
Aug 19, 2019 1:58 PM UTC

Did you change any default settings in the project wizard?

Which MCU did you select?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
JLivn
JLivnAuthor
Associate
Aug 20, 2019 8:50 AM UTC

Well, It does work for me now after installing the STM32CubeMX and initiating the project from there, it has automatically launched the IDE app with all the necessary C & H files. was it supposed to be like that?

mattias norlander
ST Technical Moderator
Aug 20, 2019 10:14 AM UTC

Well, no.

It was supposed to work also to create a new project from inside the IDE without installing any stand-alone CubeMX.

Did you follow the Quickstart Guide? I doubt that you did anything wrong. Can you re-produce it?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
JLivn
JLivnAuthor
Associate
Aug 22, 2019 6:05 AM UTC

What I can do is providing you the 'log': This computer never had any ST IDE on it before. Eclips CPP 4.11.0 is installed.

I had the previous STM32CubeIDE ver 1.0.0_2872_20190423-2022_x86_64.exe installed on June and used it to view an old job done by one of our sub contractors - which works well.

Lately I tried to start a new project afresh and that's when I bumped to this problem. I thought that something might have been missing in the installation process, so I re-download the 1.0.1 from ST site. the old project still could open, but the same problem happens for new project regardless what MCU model I select.

I have also registered for the STM32MP1 workshop, and this model is not yet supported on the IDE, so I need the MX anyway.

JLivn
JLivnAuthor
Associate
Aug 22, 2019 6:11 AM UTC
mattias norlander
ST Technical Moderator
Aug 22, 2019 12:16 PM UTC

OK - good to hear that you are at least not blocked from progressing with development.

Does this happen for any MCU? Which MCU are you using?

Did you select "STM32Cube" or "Empty" as "Targeted project type"?

The workspace should contain a .log-file in the .metadata folder. Any exceptions in this file?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
KLausL
Associate II
Oct 12, 2019 11:54 AM UTC

I am facing the same issue. Some weeks ago, I successfully created several projects for the F072 and F405/7 series. Now, project creation neither works for the F0 nor for the F4. I am not aware of any relevant changes in my system configuration. I even tried to create a new project in a completely new and empty workspace, but the error remains the same.

Steps to reproduce:

  • Start STM32CubeIDE 1.02
  • Create new workspace
  • Create new STM;32 project in workspace
  • Select STM32F072RB (the same for STM32F407VE)
  • Enter "Test" as Project Name
  • Firmware Package Version is 1.10.1
  • "Copy only the necessary library files
  • Click "Finish"

Error message ist "Creating minimal project error. Create minimal project failure: cannot read template source. Reason: Internal error. Details: Internal Error: File not found: '/C:/Users/Klaus%20Liebler/AppData/Local/Temp/stm32cubeide5842243337179599794.tmp'"

Remark: In fact, the file exists...

Thanks a lot for your help

Regards,

Klaus

TNguy.1691
Visitor II
Nov 27, 2019 6:18 PM UTC

I have the same problem. ST please help

TNguy.1691
Visitor II
Nov 27, 2019 6:19 PM UTC

Internal Error: 

File not found: '/C:/Users/Tony%20Nguyen/AppData/Local/Temp/stm32cubeide4645857718759915215.tmp'

KLausL
Associate II
Oct 15, 2019 9:15 PM UTC

The error still occurs in 1.1.0

JLivn
JLivnAuthor
Associate
Oct 18, 2019 6:33 AM UTC

Klaus

See above: I simply bypass this problem by starting every project on SMT32CubeMX. After selecting the MCU or kit and setting the I/O and timers, The MX launches the IDE automatically, then I continue the programming on the IDE. As Mattias mentioned, its not supposed to be like that, but at least I'm not stuck till the next version comes.

J.Livne

mattias norlander
ST Technical Moderator
Nov 29, 2019 7:37 AM UTC

We are totally unable to re-produce this problem. So it seems only to happen on a few environments.

If you want to use the STM32CubeIDE project wizard then please try this:

  1. Open CubeIDE in a workspace location without any spaces or non-ascii characters.
  2. Copy the necesary CubeFW folders into a location without any spaces or non-ascii characters. Then go to Window > Preferences > STM32Cube > Firmware Updater and point out the new "Firmware installation repository" folder.

We have seen spaces and non-ascii characters causing multiple problems in multiple different parts of the tools, hence it is listed as a "known problem" and not recommened. Nevertheless spaces non-ascii characters does actually work on most machines. So, feel free to try and give some feedback.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.