Skip to main content
JDoe.5
Visitor II
April 30, 2021
Question

How to work with the STM32f103c8t6 but with the cks32f103c8t6 which is the "fake blue pill" in the STMCube ide?

The blue pill I bought is not working in the STm32Cube ide. I tried using the openOCD debugger and changing the contents of the stm32f1x.cfg from

"swj_newdap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID" to

"swj_newdap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0"

Now, the IDE is showing :

Open On-Chip Debugger 0.11.0-rc2+dev-00037-g4c4dbd9 (2021-02-09-13:39)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.282353
Error: init mode failed (unable to connect to the target)

Wht shoould I do next ?

second, can I work with Keil without this error ?

This topic has been closed for replies.