Skip to main content
SWenn.1
Senior III
June 28, 2021
Question

How to use STM32CubeIDE to load hex file on target?

I am using an STLINK V3 and STM32CubeIDE V 1.6.0....I would like to load a hex file instead of the debugger .elf file onto the target. I have followed the online steps and created the hex file....

Can someone tell me the steps needed to point STM32Cube to the hex file so I can load it?

Also what is the difference between a .bin and a .hex? In TI land I am used to the .hex files

Thank you

Steve

This topic has been closed for replies.

4 replies

TDK
June 28, 2021

Using STM32CubeProgrammer instead would make it straightforward. Connect to the board, load the HEX file, and hit download.

BIN is raw data that gets stored, nothing else. No memory addresses, no offsets.

Intel HEX format includes metadata like where to put things and has some error checksum functionality. It's plaintext, you can open it in notepad.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SWenn.1
SWenn.1Author
Senior III
June 28, 2021

Thank you for the response....I understand that CubeProgrammer would work but it seems that CubeIDE is a wrapper application and should contain somewhere within to open CubeProgrammer....Do I have to download a completely separate program (that seems silly) or when I downloaded CubeProgrammer did it create a bin executable somewhere?

TDK
June 28, 2021

STM32CubeIDE is an IDE meant for compiling/debugging programs, not really meant as a standalone programmer. It contains some tools capable of flashing programs but those aren't easily exposed to the user. If you have an existing HEX file, a separate application will be easier. It is not a wrapper for STM32CubeProgrammer like it is for STM32CubeMX.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SWenn.1
SWenn.1Author
Senior III
June 28, 2021

Got it....thanks....Looks like when I downloaded and installed CubeIDE that CubeProgrammer got installed as well!

Thanks again