How to use old HAL library in CubeIDE
Hi, I have a problem using stm32f722 uC with HAL 1.16.0 and 1.16.1
I write a simple UART send project and test it with an oscilloscope (becouse it doesn't work with the target device) and discover that HAL_UART_Transmit is sending correct bytes while HAL_UART_Transmit_DMA is not. The last one corrupt a couple of byte.
So I want to check it's a bug on the library (trying old versions) or it's another problem with my implementation.
So, how could I choose an old HAL library (I have 1.15 installed) on STM32CubeIDE project generation?
Thank