Skip to main content
ASchm.1
Associate
June 6, 2020
Question

How to use __LL_ADC_CALC_TEMPERATURE?

I have a project with the STM32L053R8.

So far, so good, it works. Now I wanted to use __LL_ADC_CALC_TEMPERATURE to get the actual chip temperature - but it is not available in the __LL-list and also not in the include-file.

Can you please tell me, how to include it in the project?

Thank you

Axel

This topic has been closed for replies.

2 replies

TDK
June 6, 2020

It's defined in stm32l0xx_ll_adc.h. You need to #include this file. Make sure you're using the correct define (STM32L053xx) since it's not available on all packages.

https://github.com/STMicroelectronics/STM32CubeL0/blob/58c3ec5bb16e3475309da63f64d62efb2782594d/Drivers/STM32L0xx_HAL_Driver/Inc/stm32l0xx_ll_adc.h

"If you feel a post has answered your question, please click ""Accept as Solution""."
ASchm.1
ASchm.1Author
Associate
June 7, 2020

Hello,

thank you for your message. With the macro I got it working, but an #include "stm32l0xx_ll_adc.h" did not work. Even when I put the file in the core directory, it was not used. May be there is still something wrong.

But in the end CubeIDE is much better then Keil!

Best regards

Axel