Skip to main content
PNova.2
Associate II
August 9, 2023
Question

how to set CAN filter mask?

Hello

I'm trying to set a filter but I can't.
If I set, for example, the value 0x3 - all IDs with set bits 0 and 1 - (0x7, 0x13, 0xF, 0xF03......) pass through the filter.
I guess I didn't understand this masking. Can you tell me what I'm doing wrong?

I proceeded according to: https://www.youtube.com/watch?v=JfWlIY0zAIc

 

 sFilterConfig.FilterBank = 0;
 sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
 sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
 sFilterConfig.FilterIdHigh = 0x03<<5;
 sFilterConfig.FilterIdLow = 0;
 sFilterConfig.FilterMaskIdHigh = 0x03<<5;
 sFilterConfig.FilterMaskIdLow = 0;
 sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 sFilterConfig.FilterActivation = ENABLE;
 sFilterConfig.SlaveStartFilterBank = 14;

 

    This topic has been closed for replies.

    2 replies

    Foued_KH
    ST Employee
    August 11, 2023

    Hello @PNova.2 , 

    FilterMaskIdHigh is the Higher 16 Bits of the MASK register. The value set in this register will enable the comparison of that particular bit in the ID register to that of the incoming ID.

    When a message is transmitted on a CAN bus, its ID is compared with the filter mask to determine if it should be accepted or rejected. The bits in the filter mask that are set to 1 indicate which bits in the ID are important for filtering, while the bits set to 0 indicate which bits can be ignored.

    In summary, the filter mask is used to specify which bits in the message ID are important for filtering, and which bits can be ignored. This allows for selective filtering of messages on a CAN bus.

    Foued

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    PNova.2
    PNova.2Author
    Associate II
    August 14, 2023

    Thanks for the explanation.

    So:

    sFilterConfig.FilterIdHigh = 0x103<<5;
    sFilterConfig.FilterIdLow = 0;
    sFilterConfig.FilterMaskIdHigh = 0xFFFF<<5;//only ID in FilterIdHigh
    sFilterConfig.FilterMaskIdLow = 0;
    
    sFilterConfig.FilterIdHigh = 0x103;
    sFilterConfig.FilterIdLow = 0;
    sFilterConfig.FilterMaskIdHigh = 0x0;//any ID
    sFilterConfig.FilterMaskIdLow = 0;
    
    sFilterConfig.FilterIdHigh = 0x103;
    sFilterConfig.FilterIdLow = 0;
    sFilterConfig.FilterMaskIdHigh = 0xFF00<<5;// ID 0x100 - 0x1FF
    sFilterConfig.FilterMaskIdLow = 0;