Skip to main content
Kanna
Associate III
March 29, 2022
Question

How to resolve expression must be pointer to complete object type error?

@TDK​ 

I am getting error in below line in my code

*((uint8_t*)(CB[arr_index].baseaddress + (CB[arr_index].position*sizeof(uint8_t)))) = *((uint8_t*)data);

This error is not occuring when i am using STMCube IDE but when i am imported my project to IAR embedded workbench this line getting error

can anyone please how to resolve this problem and why it is occuring?

This topic has been closed for replies.

1 reply

KnarfB
Super User
March 29, 2022

The opposite of a complete type is an incomplete type. Like in this line, when a definition of my_unknown_struct is neither given nor included.

struct my_unknown_struct *p;

This is a valid definition of two pointer variables. In the sequel

int i = sizeof(p);
p = NULL;
p = q;
*p = 42;

The first three lines are also valid. The compiler knows everything it must know to generate code, e.g. sizeof(p) is 4.

But, the last line triggers an error, for gcc: error: invalid use of undefined type 'struct my_unknown_struct' comparable to yours.

So, the cause is probably that a complete definition of CB is not visible in IAR but in STM32CubeIDE.

hth

KnarfB