How To reset the flash control and option bytes of stm320G0XX
Hello ,
does anyone know how to reset flash control resetting method or factory resetting the stm32 microcontroller
as I am using stm320g030c8t6 in custom board which is in testing but suddenly I am not able to flash controller and getting this error which I am not able solve. Read and Write protection is off and option bytes are all ok.
-------------------------------------------------------------------
STM32CubeProgrammer v2.16.0
-------------------------------------------------------------------
Log output file: C:\Users\adity\AppData\Local\Temp\STM32CubeProgrammer_a09404.log
ST-LINK SN : 37FF6C064243393022292357
ST-LINK FW : V2J43S0
Board : --
Voltage : 2.93V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x466
Revision ID : Rev 1.1
Device name : STM32G03x/STM32G04x
Flash size : 64 KBytes
Start Address : 8000000
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0x53
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09404.srec
File : ST-LINK_GDB_server_a09404.srec
Size : 37.62 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 18]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.15.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.200.202311302303\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit